EINDHOVEN, THE NETHERLANDS AND CAMBRIDGE, UK – NXP Semiconductors and ARM [(LSE: ARM); (Nasdaq: ARMH)], will showcase the recently-announced NXP 847x/8x/9x SoC family, which is based on multiple ARM® Cortex™ processors, at CES this week. The NXP PNX847x/8x/9x represents the world’s first fully integrated 45nm Set-Top Box(STB) SoC platform incorporating multi-channel broadcast receivers. The NXP PNX847x/8x/9x utilizes the ARM Cortex-A9 MPCore™ and ARM Cortex-M3 processors, to enable a high performance, energy-efficient solution in a low-cost form factor.
“The NXP PNX847x/8x/9x platform provides an optimized system that significantly reduces the manufacturer bill-of-materials costs and power consumption enabling an improved home entertainment experience,” said Christos Lagomichos, executive vice president, business unit home, NXP Semiconductors. “With STBs and DVRs getting more and more complicated, power efficiency has been one of the major challenges for the industry. By leveraging low-power and high-performance processors from ARM, we are able to bring the next-generation HD STB and DVR features to our customers.”
The fast growing adoption of broadcast and broadband services into home entertainment equipment means that digital TVs and STBs are required to deliver higher processing performance within the tight power envelope, for compact, high-density thermally-constrained environments. The ARM Cortex-M3 processor coordinates the power management for the entire system, enabling the NXP PNX847x/8x/9x family to deliver flexible power optimization with an ultra-low power stand-by operation, enabling STB OEMs to comply with the latest EnergyStar and Voluntary Agreement.
Based on the high-performance, power-efficient ARM Cortex-A9 MPCore processor architecture, the NXP PNX847x/8x/9x delivers advanced system level performance for secure, multi-room DVR video streaming on home networks and for fast execution of Java-based STB middleware engines. Combined with NXPs rich set of hardware and DSP-based content decoding technologies, the ARM Cortex-A9 processors, with its comprehensive internet software ecosystem, delivers industry-leading performance for user interface environments, based on Adobe Flash and web browser technologies. By adopting the ARM Cortex-A9 MPCore processor for the STB market, NXP also benefits from the comprehensive and expanding ARM ecosystem.
”The showcasing of ARM technology by NXP, is a highly visible demonstration of the growing momentum behind ARM Cortex processors in set-top boxes,” said Mike Inglis, executive vice president, Processor Division, ARM. ”The combination of high-performance, low-power technology enables ARM to provide NXP with the scalable performance demanded by next-generation DVR & STB devices.”
Dedicated hardware for flexible content format decoding, alongside the ARM architecture optimizations for Javascript and Flash Player 10 components, ensures that the NXP PNX847x/8x/9x can deliver the most responsive and robust user experience for on-line VOD and other content delivered via the internet. In addition to the superb power efficiency, the PNX 847x/8x/9x family also features a 3D graphics processing unit to render advanced programming navigation user interfaces, games and other 3D content. The new NXP PNX847x/8x/9x is currently available in sample quantities.
For more information, please visit: http://www.nxp.com/applications/consumer/set-top-boxes.html
NXP will demonstrate the PNX847x/8x/9x family at the NXP booth (Wynn Hotel, Alsace 1 & 2 meeting rooms) at the Consumer Electronics Show (CES), Las Vegas, January, 7-10, 2010.
About NXP
NXP Semiconductors provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power, Digital Processing and manufacturing expertise. These innovations are used in a wide range of automotive, industrial, consumer, lighting, medical, computing and identification applications. Headquartered in Europe, the company has about 29,000 employees working in more than 30 countries and posted sales of USD 5.4 billion in 2008. News from NXP is located at www.nxp.com.
About ARM
ARM designs the technology that lies at the heart of advanced digital products, from wireless, networking and consumer entertainment solutions to imaging, automotive, security and storage devices. ARM’s comprehensive product offering includes 32-bit RISC microprocessors, graphics processors, video engines, enabling software, cell libraries, embedded memories, high-speed connectivity products, peripherals and development tools. Combined with comprehensive design services, training, support and maintenance, and the company’s broad Partner community, they provide a total system solution that offers a fast, reliable path to market for leading electronics companies. More information on ARM is available at www.arm.com.




Follow us