NXP Introduces GreenChip Resonant Controller With Integrated Power Factor Correction

February 17, 2010

GreenChip TEA1713 enables higher-efficiency power supplies

NXP Semiconductors today announced the GreenChip TEA1713 resonant half-bridge converter – the industry’s first resonant controller with integrated Power Factor Correction (PFC), capacitive mode protection and adaptive deadtime control. The high-performance GreenChip TEA1713 is a cost-effective solution enabling designers to build highly efficient, highly reliable resonant power supplies. Typical applications include power supplies above 90 W for LCD TVs, plasma TVs, PCs and slim line adapters, as well as high-quality industrial and medical power supplies.

The GreenChip TEA1713 resonant half-bridge converter complies with ENERGY STAR® requirements, delivering 90+ percent efficiency with only 50 percent of the power loss of a typical flyback converter for higher power applications. In addition, NXP offers outstanding protection features, including capacitive mode protection for resonant converters, high-frequency protection and adaptive dead-time control to ensure GreenChip benchmark robustness.

“Adapters and power supplies are becoming slimmer than ever, even for large TV displays and desktop computers, raising significant challenges for power supply designers,” said Edwin Kluter, marketing director, power solutions business line, NXP Semiconductors. “By offering an integrated resonant controller with PFC, the GreenChip TEA1713 makes it straightforward for designers to build highly efficient compact power supplies for ultra-flat notebook adapters, flat panel displays and desktop PCs. NXP’s strong heritage in High Performance Mixed Signal applications, particularly lighting, has made it possible for us introduce innovations in processing resonant-type signals while offering maximum protection in a single integrated chip.”

Key Features

The GreenChip TEA1713 is an integrated resonant controller and power factor controller for universal mains supply operation (70V to 276 VAC). The resonant half-bridge converter offers a unique combination of integrated features, including:

  • Capacitive mode protection
  • Adaptive dead-time control
  • High frequency protection (time out)
  • Over-current regulation with AC sensing
  • Two-level over-current protection with boost voltage compensation
  • Burst mode standby
  • Two-speed soft-start mechanism

Availability

The GreenChip TEA1713 is available immediately. For more information, please visit: http://www.nxp.com/pip/TEA1713T.html

About NXP Semiconductors

NXP Semiconductors provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power, Digital Processing and manufacturing expertise. These innovations are used in a wide range of automotive, industrial, consumer, lighting, medical, computing and identification applications. Headquartered in Europe, the company has about 29,000 employees working in more than 30 countries and posted sales of USD 5.4 billion in 2008. News from NXP is located at www.nxp.com.

How to search?