NXP Licenses ARM Cortex™ - M4 Processor For 32-bit Microcontroller Signal Processing Applications

February 22, 2010

Eindhoven, Netherlands, February 22, 2010 NXP Semiconductors today announced it is one of the first ARM partners to license the latest ARM® Cortex™-M4 processor. The Cortex-M4 processor is a highly efficient solution for digital signal control (DSC) applications, while maintaining the industry leading capabilities of the ARM® Cortex-M family of processors for advanced microcontroller (MCU) applications. NXP intends to use the Cortex-M4 processor for a wide range of applications which require greater flexibility and signal processing capabilities, such as motor control, automotive, power management, embedded audio and industrial automation applications. NXP will demonstrate these DSP extensions at Embedded World, Nuremberg (March 2 - 5, 2010) to highlight Cortex-M4‘s DSP capabilities. NXP‘s booth number: Hall 12, 218.

“The addition of the ARM Cortex-M4 processor to our ARM Cortex portfolio complements our Cortex-M3 and Cortex-M0 processor-based devices and enables us to provide an end to end solution to the MCU community,” said Geoff Lees, vice president and general manager, microcontroller product line, NXP Semiconductors. ‘With NXP focusing on High Performance Mixed Signal technologies and building on our close cooperation with ARM, we look forward to bringing a Cortex-M4 based MCU to the market, very soon.”

The Cortex-M4 processor is the latest member of the Cortex-M family and is the most efficient ARM processor ever for digital signal control applications. It provides an optimal blend of high-performance digital signal processing features like single-cycle MAC, single instruction multiple data (SIMD) techniques, saturating arithmetic, and a floating point unit, with essential microcontroller features such as integrated interrupt control, low power modes, low cost debug and ease of use. More information is available at: www.nxp.com.

Forward-looking Statements
This release may contain certain forward-looking statements with respect to the financial condition, results of operations and business of NXP and certain plans and objectives of NXP with respect to these items. By their nature, forward-looking statements involve risk and uncertainty because they relate to events and depend on circumstances that will occur in the future and there are many factors that could cause actual results and developments to differ materially from those expressed or implied by these forward-looking statements.

For further press information, please contact:

USA:
Rebecca Samuel
Tel. +1 408 474 8769
Rebecca Samuel

Europe
Terry Chiang
Tel. +31 40 2725162
Terry Chiang
  APAC:
Mark Chisholm
Tel. +1 408 474 8769
Mark Chisholm

Greater China:
Jannet Chen
Tel. +86-21-22055883
Jannet Chen

How to search?