NXP Semiconductors Announces High Speed Converter Interoperability / Interworking with Xilinx FPGAs

February 11, 2010

Eindhoven, The Netherlands, February 11, 2010 - NXP Semiconductors has announced that its CGV™ series of JESD204A-compliant data converters are now interoperable with Xilinx® high performance Virtex®-6 FPGAs and low-cost Spartan®-6 FPGA families. Assured interoperability and interworking between programmable logic devices and high-speed converters is a critical acceptance criterion for equipment designers, because it eliminates risk and cost associated with project schedules.

The new JESD204A-compliant CGV converters from NXP are suitable for cellular base stations and other wireless communication infrastructure equipment, as well as medical, instrumentation and military/aerospace applications. NXP has developed dedicated CGV ADC and DAC interoperability demo and high performance data acquisition reference design / evaluation boards based on Virtex FPGAs which are available to customers immediately. NXP also offers CGV ADC and DAC demo boards with the FMC interconnect interface for use with Virtex-6 FPGA and Spartan-6 FPGA-based evaluation boards. NXP first publically demonstrated JESD204A CGV data converters interworking with Virtex FPGAs in June 2009 at the IEEE MTT 2009 International Microwave Symposium in Boston. NXP has more than 12 months of JESD204A interworking experience with Xilinx FPGAs, an important consideration for prospective customers.

“NXP Semiconductors is pleased to extend this assured interoperability to our CGV customers, many of whom are interested in using the latest Xilinx FPGAs in their system designs”, said Maury Wood, senior director and product line manager, high speed Converters, NXP Semiconductors. ‘NXP offers several demo boards based on Xilinx Virtex FPGAs which offer clear evidence of this device interoperability. We‘ve also demonstrated interworking during the worldwide Avnet X-fest events beginning in October 2009”, said Wood.

“Through strong collaboration with NXP, we are able to deliver seamless interoperability between our latest FPGA families and NXP‘s data converters”, said Manuel Uhm, director of wireless communications at Xilinx. “Available Xilinx FPGA-based JESD204A reference designs ease the transition from IO limited parallel LVDS based data converters to Serdes-based multi-module high performance data converters while reducing board complexity and system cost,” said Uhm.

CGV™ (Convertisseur Grande Vitesse) designates NXP‘s compliant, superset implementation of the JEDEC JESD204A interface standard, with enhanced rate (4.0 Gbps typical), enhanced reach (100 cm typical), enhanced features (multiple DAC synchronization) and assured FPGA interoperability. Specifically, NXP offers enhancements in terms of transceiver rate (up to 4.0 Gbps versus the standard rate of 3.125 Gbps, a 28% increase), and transmitter reach (up to 100 cm versus the standard reach of 20 cm, a 400% increase). The enhanced CGV features include Multi Device Synchronization (MDS) for the DAC1408D series of D/A Converters, which is not specified, but informatively discussed in the JEDEC specification. NXP has implemented this optional feature to enable LTE MIMO base station and other advanced multi-channel applications. NXP‘s implementation of MDS enables up to sixteen DACs data streams to be sample synchronized and phase coherent.

Virtex®-6 and Spartan®-6 FPGAs provide the programmable silicon foundation for Xilinx® Base-level, Domain-specific, and Market-specific Targeted Design Platforms that enable designers to accelerate innovation and improve differentiation across a wide range of markets and applications. Built for high-performance, compute-intensive applications, Virtex-6 FPGAs deliver over 1Tbps of digital signal processing bandwidth and more than 11Gbps of serial connectivity that is fully scalable and optimized to reduce overall system power consumption. Spartan-6 FPGAs offer an optimal balance of cost, power, and performance that for the first time brings low power and ubiquitous high-speed connectivity to price-sensitive, high-volume markets.

About NXP Semiconductors

NXP Semiconductors provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power, Digital Processing and manufacturing expertise. These innovations are used in a wide range of automotive, industrial, consumer, lighting, medical, computing and identification applications. Headquartered in Europe, the company has about 29,000 employees working in more than 30 countries and posted sales of USD 5.4 billion in 2008. News from NXP is located at www.nxp.com.

Forward-looking Statements
This release may contain certain forward-looking statements with respect to the financial condition, results of operations and business of NXP and certain plans and objectives of NXP with respect to these items. By their nature, forward-looking statements involve risk and uncertainty because they relate to events and depend on circumstances that will occur in the future and there are many factors that could cause actual results and developments to differ materially from those expressed or implied by these forward-looking statements.

For further press information, please contact:

USA:
Rebecca Samuel
Tel. +1 408 474 8769
Rebecca Samuel

Europe
Terry Chiang
Tel. +31 40 2725162
Terry Chiang
  APAC:
Mark Chisholm
Tel. +1 408 474 8769
Mark Chisholm

Greater China:
Jannet Chen
Tel. +86-21-22055883
Jannet Chen

How to search?