NXP, STMicroelectronics, Trusted Logic and Stollmann to Promote Hardware-Independent NFC API for Android™

June 01, 2010

Geneva, Switzerland, and Eindhoven, The Netherlands, June 1st, 2010 – Market-leading NFC vendors STMicroelectronics (NYSE: STM) and NXP today announced, in conjunction with Trusted Logic and Stollmann, that the companies are to promote a common hardware-independent API (Application Programming Interface) for NFC (Near Field Communication) applications on mobile phones and other devices running Android™.

The companies will release an update of their recently published Android APIs to the community as a proposal for a mutual standard. The common NFC API is seen as a central resource enabling developers to create NFC applications to be distributed through app stores. This will enable mobile phone users to access a new range of contactless applications capable of conveniences such as mobile payments, transport and event ticketing as well as data sharing directly from their Android™ phone.

The API is a result of consultations with various eco-systems partners, including mobile network operators, handset manufacturers and NFC controller providers. It is supported by protocol stacks that are compatible with major NFC chip platforms from STMicroelectronics and NXP and can be used for mobile phones, mobile Internet devices, PCs and more.

“NXP has always been at the forefront of mobile transactions and is committed to enable NFC on Android-based devices jointly with other industry leaders,” said Henri Ardevol, General Manager Secure Transactions, NXP Semiconductors. “We are pleased to collaborate with STMicroelectronics, Stollmann, Trusted Logic and other partners to define and standardize a truly open NFC API for Android.”

“Technical collaboration between leading NFC-protocol stack vendors and NFC-chip manufacturers is both a major and necessary step towards massive adoption of NFC in the Android environment,” said Laurent Degauque, Telecom & NFC Marketing Manager, STMicroelectronics. “This joint and open approach, shared by four key players, will pave the way for the successful deployment of NFC technology and create increased confidence for customers.”

Philippe Dubois, General Manager Professional and Consumer Devices, Trusted Logic, comments: “A single common API agreed on by the major solution providers is essential to develop the NFC ecosystem within Android and meet our customers’ expectations.”

“A well maintained protocol stack that conforms to standards and supports the features of NFC is the key to make NFC a successful and flexible technology and to attract developers to write applications for NFC on Android a common API is another one,” said Christian Lührs, General Manager, Stollmann.

The API specification will be accessible via a single email request to NFCforAndroid@trusted-logic.com and nfc@stollmann.de. An Apache License 2.0 model was selected in order to provide a legal framework to new contributions.

About NXP Semiconductors

NXP Semiconductors provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. Headquartered in Europe, the company has approximately 28,000 employees working in more than 25 countries and posted sales of USD 3.8 billion in 2009.

About STMicroelectronics

STMicroelectronics is a global leader serving customers across the spectrum of electronics applications with innovative semiconductor solutions. ST aims to be the undisputed leader in multimedia convergence and power applications leveraging its vast array of technologies, design expertise and combination of intellectual property portfolio, strategic partnerships and manufacturing strength. In 2009, the Company’s net revenues were $8.51 billion. Further information on ST can be found at www.st.com.

How to search?