Unterpremstaetten, Austria (November 30, 2010) – austriamicrosystems (SIX: AMS), a leading global designer and manufacturer of high-performance analog ICs, and NXP Semiconductors N.V. (Nasdaq: NXPI), a leading provider of RFID solutions, today announced that they have jointly developed the first in a range of reference solutions for product authentication in embedded consumer applications. Leveraging the AS399x UHF RFID Reader IC, and the UCODE G2iL series, the reference design delivers the industry’s lowest power consumption, lowest solution cost, lowest complexity and highest level of integration - a combination unmatched anywhere in the world.
Applications which can best benefit from this new reference solution are those where authentication of consumables plays an important role, for example to ensure product quality and consumer safety with items such as vacuum cleaner bags, water filters, and beverage concentrates. With such RFID functionality, equipment manufacturers would be able to warn users about health risks, as well as about threats of product malfunction in cases when non-authentic consumable is used. And in cases when end user ignores such warnings and willingly feeds the equipment with consumable of unknown or non-approved quality, the equipment manufacturer would have the option to void equipment's warranty.
NXP and austriamicrosystems join forces for a one-stop-shop turnkey solution in these applications because the two companies' products and expertise are very complementary and include over 20 years of RFID industry experience on both sides. By leveraging these capabilities, this collaboration enables both partners to develop state-of-the-art total RFID system solutions suitable for authentication applications in consumer products.
Besides low power and low complexity, these authentication systems require very low external code load, meaning it is easy to use a host controller or a low-end microcontroller. NXP’s G2iL and G2iL+ products - in addition to offering password protected features, privacy commands and anti-tampering functions - also offer high chip sensitivity which leads to high read reliability even with extremely small tags. Furthermore, with austriamicrosystems' reference designs for Ultra Low Cost EPC Gen 2 compliant UHF RFID Reader systems with lowest reader BOM, applications that have previously been out of reach due to cost restraints now become addressable.
"The cost versus performance considerations for embedded applications in consumer products mean that we are the only real choice on the market at the moment," said Kambiz Dawoodi General Manager Consumer & Communications, austriamicrosystems. "This collaboration with NXP means we now can also provide a solution with the most competitive tag silicon on the market."
NXP's General Manager for Tagging and Authentication Chris Feige added: "With NXP's expertise at RFID Applications and System Center, and in conjunction with austriamicrosystems' UHF reader competences, brand owners will now have one-stop-shop partner for embedding RFID systems into consumer products even in cases of very demanding requirements on cost, performance and physical space. Such RFID-enabled authentication of consumable products leads to revenue, brand and end-user protection."
Learn more about the collaboration and the expertise in RFID and visit austriamicrosystems and NXP at the RFID/USN Korea 2010 - 2010/12/02 - 2010/12/04 Seoul, Korea Booth F120.
About NXP Semiconductors
NXP Semiconductors N.V. (Nasdaq: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. Headquartered in Europe, the company has approximately 28,000 employees working in more than 25 countries and posted sales of USD 3.8 billion in 2009.
About austriamicrosystems
austriamicrosystems is a leading designer and manufacturer of standard and customized high-performance analog ICs in the areas of power management, sensors & sensor interfaces and mobile infotainment. Complemented by its full service foundry services, the company focuses on the communications, industrial & medical and automotive markets. austriamicrosystems leverages almost 30 years of expertise in low power and high accuracy to provide industry-leading products, operating worldwide with more than 1,000 employees with its own state-of-the-art manufacturing and test facilities. austriamicrosystems is listed on the SIX Swiss Exchange in Zurich (ticker symbol: AMS). For more information, visit www.austriamicrosystems.com
For further information
| Press Contact austriamicrosystems AG Ulrike Anderwald Marketing Communications Manager Tel: +43 (0) 3136 500 5856 Fax: +43 (0) 3136 500 5420 press@austriamicrosystems.com www.austriamicrosystems.com |
Technical Contact austriamicrosystems AG Mark Dickson Product Marketing Manager Tel: +43 (0) 3136 500 5916 Fax: +43 (0) 3136 500 5420 mark.dickson@austriamicrosystems.com www.austriamicrosystems.com |
| NXP Semiconductors: Europe: Stuart Gill Tel. +44 208 846 0758 Stuart.Gill@text100.co.uk Americas: Rebecca Samuel Tel. +1 408 474 8769 rebecca.samuel@nxp.com |
NXP Semiconductors: Greater China: Fei Wang Tel. +86 10 8520 8307 fei.wang@nxp.com APAC: Anne Suzan Ariens Tel: +65 6882 4416 anne.suzan.ariens@nxp.com |




Follow us