NXP High-Speed Converters Now Interoperable With Nujira OpenET Envelope Tracking Solutions

January 20, 2011

Eindhoven, Netherlands, January 20, 2011: NXP Semiconductors N.V. (Nasdaq: NXPI) today announced that its CGV™ series of JESD204A-compliant data converters are now interoperable with Nujira’s OpenET envelope tracking (ET) and digital pre-distortion (DPD) solutions. Nujira is a leader in commercial-grade envelope tracking modulators for 3G and 4G wireless infrastructure applications, and is the founder of the OpenET Alliance. NXP CGV analog-to-digital converters (ADCs) and digital-to-analog converters (DACs) are the first in the industry to implement the JEDEC JESD204A serial interface, which dramatically reduces the number of interconnect signals between data converters and VLSI logic devices, and enables synchronous bonding of multiple data converter channels or lanes. Nujira’s next-generation Coolteq-h Envelope Tracking modulators now also support JESD204A as an interface option.

Facts / Highlights:

  • The NXP high-speed CGV ADCs and DACs have been tested for interoperability using Nujira’s OpenET development system, which implements envelope tracking and DPD functionality.
  • Assured interoperability and interworking between programmable logic devices and high-speed converters is a critical acceptance criterion for equipment designers, because it reduces risk and cost associated with project schedules.
  • Envelope tracking enables high-efficiency power amplifiers for wireless infrastructure to dynamically reduce the electrical power to a radio transmitter at times of low signal amplitude, and increase it when a powerful signal is required.
  • Nujira’s DPD technology has been developed to improve signal quality while maintaining high efficiency, which is critical for modern base stations.
  • The JESD204A-compliant CGV converters from NXP are suitable for cellular base stations and other wireless communication infrastructure equipment, as well as medical, instrumentation and military/aerospace applications.
  • The NXP CGV (Convertisseur Grande Vitesse) series also delivers a number of enhancements over and above standard implementations of JESD204A, including:
    • Enhanced transceiver rate up to 4.0 Gbps typical
    • Enhanced transmitter reach up to 100 cm typical
    • Enhanced features including Multi Device Synchronization (MDS) and pseudo random bit sequence (PRBS) generation for robustness validation
    • Assured FPGA interoperability

Supporting Quotes:

  • “NXP is pleased to work with Nujira to establish assured JESD204A interoperability. This collaborative activity further underpins NXP’s leadership in JEDEC JESD204A technology,” said Maury Wood, product line manager, High Speed Converters, NXP Semiconductors.
  • “Nujira’s decision to utilize the industry-standard JESD204A interface for our next generation of Coolteq-h Envelope Tracking modulators was driven by widespread adoption by leading ADC and DAC providers. This interoperability testing with NXP is an important step in reducing risk and time-to-market for our customers.” said Simon Whittle, design center manager, Nujira.

Links

About NXP Semiconductors

NXP Semiconductors N.V. (Nasdaq: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. Headquartered in Europe, the company has approximately 28,000 employees working in more than 25 countries and posted sales of USD 3.8 billion in 2009.

How to search?