Eindhoven, Netherlands and Beijing, China, March 24, 2011 - At CCBN2011 today, NXP Semiconductors N.V. (NASDAQ: NXPI) announced new additions to its Ultra High Frequency (UHF) and FM broadcast product portfolio, including the BLF888B transistor. Configured as a Doherty power amplifier, the BLF888B achieves breakthrough 50 percent DVB-T efficiency, offering significant reductions in the power consumption of UHF broadcast systems.
NXP’s latest UHF and FM LDMOS power transistors offer cost-effective solutions for specific power levels previously unavailable, using thermally optimized transistor designs. Innovations include:
- Improved ruggedness over the full UHF frequency band from 470 to 860 MHz, which enables the application to withstand extreme mismatches
- Lowest thermal resistance in the market (Rth = 0.15 K/W) for BLF888A and BLF888B
- 50 percent efficiency using the BLF888B in a Doherty configuration
YingHao Zhuo, NXP Semiconductors senior regional marketing manager for RF power and base stations in Greater China, said: “With our latest products, NXP is addressing market demand for improved higher drain efficiency, higher output power and improved frequency bandwidth with innovative UHF Broadcast DVB-T solutions.”
Highlights of the new UHF products are:
- BLF888A transistor - 125 Wavg DVB-T with 32 percent efficiency, 21 dB gain, capable of covering the full UHF band
- BLF888B transistor - optimized for use in a Doherty configuration, achieving 50 percent efficiency at 120 W output power and 18 dB gain
- BLF879P transistor - 95 Wavg DVB-T with 32 percent efficiency, 20 dB gain, capable of covering the full UHF band
- BLF884P transistor - 70 Wavg DVB-T with 33 percent efficiency, 21 dB gain, capable of covering the full UHF band
Characteristics of the new FM product:
- BLF178P transistor - optimized for FM radio transmitters in terms of cost/performance, delivering 1kW CW with 75 percent efficiency at 108 MHz and 26.5 dB gain
Further information on the latest additions to NXP’s UHF and FM broadcast portfolio will be available this week at CCBN2011, the China Content Broadcasting Network Exhibition in Beijing, booth 1B025, 26. Data sheets, pricing and samples are available on request. Information on NXP’s comprehensive portfolio of High Performance RF solutions for broadcast is available at: http://www.nxp.com/campaigns/high-performance-rf/
About NXP Semiconductors
NXP Semiconductors N.V. (Nasdaq: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 30 countries, NXP posted revenue of $4.4 billion in 2010. For more information visit www.nxp.com.
For further press information, please contact:
USA:
Rebecca Samuel
Tel. +1 408 474 8769
rebecca.samuel@nxp.com
Europe:
Eureka Endo
Tel: +44 795 828 7483
eureka.endo@nxp.com
APAC:
Hui Yun Chen
Tel: +65 6882 4146
huiyun.chen@nxp.com
Greater China:
Jannet Chen
Tel: +86 21 22055883
jannet.chen@nxp.com






Follow us