NXP Delivers Industry’s First 10 Gbps CMOS Multiplexer/Demultiplexer Switch

March 15, 2011

CBTL02043 supports high-bandwidth systems while minimizing power consumption

Eindhoven, Netherlands and San Jose, California, March 15, 2011 – NXP Semiconductors N.V. (Nasdaq: NXPI) today announced the availability of the CBTL02043, a multiplexer/demultiplexer (mux/demux) switch featuring the highest speed implementation in the industry. Providing switching speeds of up to 10 Gbps, the CBTL02043 maintains low power consumption and low power loss, and is designed to support rapidly evolving high-speed computing standards for desktop, mobile and enterprise systems such as PCIe Gen3, USB3.0, DisplayPort v1.2 and SAS/SATA 6 Gbps.

The CBTL02043 can switch two differential signals to one of two locations, while providing low signal attenuation. Using NXP’s high-bandwidth CMOS pass-gate technology, the 2:1 mux/demux switch minimizes switch impedance and allows for expansion of existing high-speed ports, contributing to higher bandwidth and lower insertion loss. Providing minimized channel-to-channel skew and crosstalk, the CBTL02043 is delivered in a very small form factor supporting two separate pinout configurations, optimized to match different application layouts.

Facts / Highlights:

Key features of the NXP CBTL02043A/B high-speed multiplexer/demultiplexer switch:

  • Switching speeds of up to 10 Gbps
  • Support for standards such as PCIe Gen3, USB3.0, DisplayPort v1.2 and SAS/SATA 6 Gbps
  • High bandwidth at 10 GHz at -3dB
  • Low return loss at -20 dB at 4 GHz
  • Shutdown pin (XSD) for power-saving mode
  • Low crosstalk at -35 dB at 4 GHz
  • Low off-state isolation at -20dB at 4 GHz
  • Available in a very thin DHVQFN20 package (20 terminals, 2.5 x 4.5 x .85 mm)

Supporting Quote:

  • “NXP is first to release a CMOS multiplexer/demultiplexer switch supporting speeds of up to 10Gbps,” said Grahame Cooney, general manager, high speed interface, NXP Semiconductors. “This breakthrough helps our customers get ahead of the curve by supporting high-bandwidth applications, addressing evolving digital interface standards, and minimizing power consumption.”

Availability

The CBTL02043 is available immediately and will be showcased at the Digitimes High Speed Interface Tech Forum in Taiwan. Pricing is US $.90 for 1k to 10k units.

Links

  • CBTL02043A/B product information page
  • NXP interface products

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 30 countries, NXP posted revenue of $4.4 billion in 2010. For more information visit www.nxp.com.

For further press information, please contact:

USA:
Rebecca Samuel
Tel. +1 408 474 8769
rebecca.samuel@nxp.com


Europe:
Eureka Endo
Tel: +44 795 828 7483
eureka.endo@nxp.com


APAC:
Hui Yun Chen
Tel: +65 6882 4146
huiyun.chen@nxp.com


Greater China:
Jannet Chen
Tel: +86 21 22055883
jannet.chen@nxp.com

How to search?