Eindhoven, Netherlands and San Jose, California, April 27, 2011 – NXP Semiconductors N.V. (NASDAQ: NXPI) today announced CGVxpress™, an important extension to its high speed data converter technology portfolio and the next generation of the CGV™ high speed serial interface announced in 2009. The newly announced CGVxpress will be used in future NXP ADC and DAC product families. The first demonstration of CGVxpress will occur at booth #420 of the IEEE International Microwave Symposium (MTT-S) held June 7-9, 2011 in Baltimore, Maryland. NXP will showcase a 4.5 Gbps CGVxpress transmitter interworking with an industry standard FPGA over a 20 cm differential data lane.
CGVxpress (Convertisseur Grande Vitesse or High Speed Converter) interface technology is ideal for: wireless infrastructure (WIFR), industrial, scientific, medical (ISM), and aerospace and defense (A&D) applications, where high bandwidth, sample accurate lane synchronization and deterministic latency are critically technical requirements. The CGVxpress feature set also includes support for Multi-Device Synchronization (MDS). MDS solves tough system synchronization and latency challenges in many digital communications system applications, including LTE and LTE-Advanced MIMO radio base stations.
“NXP continues to strengthen its leadership position in high-speed serial interfaces with a major enhancement to CGV, and set the pace for data converter innovation,” said Maury Wood, product line general manager, high speed converters, NXP Semiconductors. “CGVxpress delivers value that goes beyond traditional parallel interfaces, providing dramatic enhancements to ease-of-use, cost benefits and system architecture. The technology and performance enhancements enabled by CGVxpress will drive this serial interface into ubiquitous adoption by data acquisition system engineers worldwide.”
The CGV interface currently appears on several products in NXP’s high speed ADC and DAC product line - including the ADC1413D and DA1408D product families.
Additional Benefits
- CGVxpress dramatically reduces the number of interconnect signals between the data converters and logic devices
- Solves a major base station system design challenge by synchronously bonding multiple data lanes with sample level accuracy
- CGVxpress facilitates significantly reduced PCB design and manufacturing complexity, impacting both NRE costs and marginal production costs; systems can often be implemented using fewer PCB layers as compared to traditional parallel interfaces
About NXP High Speed Data Converters
NXP is a leader in high performance mixed-signal IC products and the recognized leader in SERDES-based serial interfaces for high speed converters. NXP offers a broad selection of high-speed data converters, with digital interfaces including JESD204A compliant CGV, CMOS LVCMOS and LVDS DDR interfaces. These high speed converters are suitable for wireless infrastructure, industrial, scientific, medical, aerospace and defence applications.
Availability
NXP offers several CGV products, including the ADC1413D and DAC1408D, both of which are currently available. Specific products utilizing CGVxpress technology at 4.5 Gbps and higher will be announced later this year.
Further information about NXP’s CGVxpress technology is available at: http://www.nxp.com/campaigns/fasttrackyourdesign/
Information about NXP’s high speed data converter portfolio is available at: http://www.nxp.com/products/data_converters/
About NXP Semiconductors
NXP Semiconductors N.V. (Nasdaq: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 30 countries, NXP posted revenue of $4.4 billion in 2010. For more information visit www.nxp.com.






Follow us