NXP Small-Signal MOSFETs Set New Benchmark in RDS(on)

June 14, 2011

New portfolio enables increased power efficiency for mobile computing, communications and other consumer applications

Eindhoven, Netherlands and Hamburg, Germany, June 14, 2011 – NXP Semiconductors N.V. (NASDAQ: NXPI) today announced a new family of small-signal MOSFETs delivering breakthrough low RDS(on) performance. The low RDS(on) P-Channel and N-Channel MOSFETs enable lower power consumption for consumer electronics applications such as notebooks, tablets, handsets, e-readers, set-top-boxes and LCD TVs. These high-efficiency MOSFETs are available in high-volume SOT23 and SOT457 packages with a compact 3-mm x 3-mm footprint, allowing design engineers to replace larger package types with significantly smaller solutions offering similar or better on-resistance.

Facts / Highlights:

  • The PMV16UN, one of the new N-Channel MOSFETs from NXP, delivers an ultra-low RDS(on) value of (18 mOhm max @VGS = 4.5 V) in SOT23.
  • NXP’s latest portfolio of small-signal MOSFETs offers a 20-percent increase in power efficiency compared to previous Trench MOSFET generation types.
  • Parts are available immediately for US $1.20 in units of 1,000.
  • A total of 70 types of small-signal MOSFETs will be released in 2011.

Supporting Quote:

  • “Our new small-signal MOSFETs have set new benchmarks in low on-state resistance in SOT23, enabling higher efficiency in much smaller form factors in an increasingly competitive consumer electronics market,” said Jens Schnepel, product marketing manager, transistors, NXP Semiconductors.

Links:

About NXP

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.4 billion in 2010.

How to search?