At this year’s European Microwave Week (EuMW), technical experts from NXP Semiconductors will be participating in numerous conference sessions and workshops highlighted below.
EuMW 2011 will be held from 9th – 14th October in Manchester, UK, and is an industry-leading event where manufacturers, institutes and industry bodies have the opportunity to discuss relevant issues in Microwave, RF, Wireless, Defense / Security and Radar. NXP will be showcasing the latest High Performance RF technologies and solutions in Booth 313.
One highlight this year is the industry panel on “Selecting the Right Technology for High Power Military Applications,” which will be taking place on Wednesday 12th October from 15.00 to 16.30 BST. Mark Murphy, director of RF Power products at NXP Semiconductors, will be speaking.
For more information on NXP’s High Performance RF business line, visit http://www.nxp.com/high-performance-rf
Workshops
Sunday 9th October
- Workshop W 06: Foreseen Technologies towards Cognitive Transceivers: Critical blocks, hardware design and algorithms
- 09:50 – 10:30 - Software defined radio/cognitive paradigms, emerging applications and silicon: Key Technological Issues
- 14:45 – 15:20 - High efficiency PA towards SDR/CR: review and perspective of Doherty and LINC architectures
- Workshop W 11: Applications of RF MEMS
- 09:40 – 10:10: Towards Smaller Thin-fi lm Packaged Ohmic MEMS Switches
Conferences
Tuesday 11th October
- EuMIC Conference, Charter 3, High Efficiency Power Amplifier
- 08:50-09:10 - A Compact 65W 1.7-2.3GHz Class-E GaN Power Amplifier for base stations
- EuMIC Conference, Charter 6, Silicon microwave circuits
- 08:50 – 09:10 - A 10 GHz Integrated Single Sideband Upconverter in 0.25 µm BiCMOS Technology
- 09:30 – 09:50 - A Low Power 9.75/10.6GHz PLL in SiGe:C BiCMOS for Ku-Band Satellite LNBs
- EuMIC Conference, Charter 1, Frequency Synthesis and Millimeter-Wave Receivers
- 13:40 – 15:00 - Frequency Synthesis and Millimeter-Wave Receivers
- EuMIC Conference, Charter 2, Silicon and III-V Based Technologies for Advanced Sub-mm Wave Applications
- 14:00 – 14:20 - Design of Antenna on-Chip, Antenna-onPackage and Detectors from Microwave and THz Frequency Range in SiGe-C Technology
- EuMIC Conference, Charter 6, Passive circuits based on advanced technologies
- 15:40 – 16:00 - A Transformer for HighPower RF Applications Using Bondwires in Parallel
- EuMC Poster Sessions 12:30 – 18:00
- EuMIC Poster 01-10: Broadband Digitization for Cable Tuners Front-End
- EuMIC Poster 02-37: Effects of Inter-Chip and Intra-Chip Electromagnetic Interferences on PLL Frequency Pulling and Spurs
- EuMIC Poster 02-38: Design and Verification of Built-in-Self-Test (BIST) for RF, and Microwave Applications
Wednesday 12th October
- EUMC Conference: Communication Subsystems
- 10:50 – 11:10 - Linearity Considerations for Multi-Standard Cellular
- “Radar Challenges & Solutions” Industry Panel session, Charter 1
- 15.00 – 16.30 - Selecting the Right Technology for High Power Military Applications
About NXP
NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.4 billion in 2010. For more information visit www.nxp.com




Follow us