Latest videos

  • NXP Presents Android Open Accessory Application (A...

    youtube video

    NXP Presents Android Open Accessory Application (AOAA) Kit with Embedded Artists


Embedded Artists and NXP Release Industry’s First Android Open Accessory Development Kit on ARM Cortex-M Architecture

February 28, 2012

Gateway-centric design includes interfaces for CAN, Ethernet and 802.15.4 wireless networks

At Embedded World 2012 today, Embedded Artists AB and NXP Semiconductors N.V. (NASDAQ: NXPI) introduced a powerful new Android™ Open Accessory Application (AOAA) development kit with two high-performance NXP microcontrollers based on the 32-bit ARM® Cortex™-M architecture. Featuring the NXP LPC1769 and the LPC11C24 microcontrollers, the Embedded Artists AOAA kit makes it easy for designers to develop, evaluate and prototype more complex accessories for Android smartphones and tablets. The board’s unique gateway-centric design includes Ethernet, CAN and IEEE 802.15.4 interfaces as well as a remote CAN node, enabling designers to develop highly advanced accessories not only for consumer applications, but also for home, building and industrial automation applications requiring different types of connectivity.

“Our new AOAA development kit, built in collaboration with NXP, opens a new world of possibilities for Android accessory designers,” said Maria Hall, managing director, Embedded Artists. “By taking advantage of one of the many connectivity options, the Android accessory is no longer simply an isolated system. Instead, it can serve as a gateway to a networked system for use in a wide range of very powerful applications.”

Two High-Performance NXP Cortex-M Microcontrollers

The on-chip full-speed USB transceiver of the LPC1769, a 120-MHz Cortex-M3 based microcontroller, provides the interface to the Android mobile device. The LPC1769 also supports USB device mode, helping to “future proof” designs, should Android devices support USB host mode in the future. Other features of the LPC1769 include 512 KB flash and 64 KB on-chip SRAM; Ethernet MAC; a CAN 2.0B controller; an 8-channel, 12-bit ADC; a 10-bit DAC; digital connections including UART/SPI /I2C, numerous timers and PWMs; and low-power capabilities.

The LPC11C24 microcontroller, based on the Cortex-M0 processor, provides remote CAN node capabilities to the AOAA kit and is connected to the LPC1769 via an on-board CAN network. The LPC11C24 allows designers to develop industrial control applications using CAN, by taking advantage of control functionality for temperature, light and other sensors, which are built directly on the AOAA kit.

Extensive Software Support

Users of the Embedded Artists AOAA kit will receive all the software needed to get started with their designs including reference applications to test and build Ethernet, CAN and wireless functions. The royalty-free reference applications, which are available for download from Embedded Artists, include 1) controlling and monitoring the AOAA board from an Android device; 2) using the Android device to detect, control and monitor CAN nodes in a CAN network; and 3) using the Android device to detect, control and monitor Xbee nodes.

The AOAA kit is also a fully extensible development tool, as plug-in modules from Embedded Artists can be added quickly and easily. Further, free software support libraries are available for download at LPCware.com, including the emWin graphics library, nxpUSBlib, lwIP TCP/IP stack and more.

“With a majority of smartphones using Android today, the Android Open Accessory standard provides a critical link between phones, tablets and other mobile computing devices, and the embedded systems that are pervasive in our daily lives,” said Gordon Cooper, international product marketing manager, microcontroller business line, NXP Semiconductors. “Building on our successful collaboration on LPCXpresso, we’ve worked very closely with Embedded Artists to create an easy-to-use development kit that will help to take Android accessories to the next level.”

Availability

The AOAA Kit for Android is available from Embedded Artist for US $79.99 at www.embeddedartists.com and from NXP through approved distributors. NXP will showcase the Embedded Artists AOAA kit this week at Embedded World in Nuremberg, Germany (Hall 4A, Booth 222).

Links

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.2 billion in 2011. Additional information can be found by visiting www.nxp.com.

About Embedded Artists

Embedded Artists is a leading provider of products and services around prototyping, evaluation and OEM platforms for NXP-based embedded systems. Embedded Artists’ Developer's Kits, OEM boards and customization services ensure simpler and shorter design and development times, speeding up time to market and driving down costs. The company was founded year 2000 and is located in Sweden. For more information visit http://www.embeddedartists.com.

How to search?