Latest videos

  • Ambient lighting NXP UJA1018 networking solution...

    youtube video

    Ambient lighting NXP UJA1018 networking solution


NXP Enables Cost-Efficient and Flexible LED Ambient Lighting Solutions for the Car

July 19, 2012

UJA1018 simplifies configuration of interior lighting and offers car manufacturers and consumers great customization options

Eindhoven, Netherlands, July 19, 2012 – NXP Semiconductors N.V. (NASDAQ: NXPI) – the world’s largest supplier of in-vehicle networking semiconductors – today introduces the UJA1018, a compact integrated solution that supports cost-efficient and flexible LED ambient lighting applications in vehicles. The UJA1018 is designed for LIN networks (Local Interconnect Networks) and is the first ASSP (Application Specific Standard Product) for ambient lighting with Node Position Detection. This enables LIN addresses of LED modules to be individually programmed after being installed in the car, rather than during module manufacturing. Ambient LED lighting is increasingly popular in the automotive industry. Car manufacturers are using it as a differentiator to enhance the driving experience. It also enables OEMs to emphasize their car brand via the color and styling of the interior lighting, while car dealers can offer consumers the option of customizing the lighting settings.

Whereas interior LED modules are currently programmed during the module manufacturing process, with NXP’s new Node Position Detection method, based on an integrated LIN switch, all LED modules can be individually configured even after being mounted in the car. This offers new levels of flexibility while drastically reducing manufacturing logistics and costs.

The UJA1018 integrates all analog functions to create a compact ambient lighting solution, including LIN transceiver, LIN switch for Node Position Detection, voltage regulator for microcontroller and drivers for 3-color LED. In addition, the compact HVSON package enables the creation of small form factor modules. The UJA1018 fulfills the robustness requirements from the OEMs and also meets the SAE J2602 and LIN conformance.

“With the UJA1018 and its unique Node Position Detection technology based on LIN switch, NXP enables car OEMs to offer personalized ambient lighting solutions to end consumers. At the same time it saves system costs and simplifies logistics for both OEMs and Tier1 suppliers,” says Toni Versluijs, general manager of In-Vehicle Networking, NXP Semiconductors. “This underpins our leadership position as the de-facto In-Vehicle Network solution provider and our commitment to connect the car in present and in future”.

Dr. Herbert Wambsganß, head of development at HELLA Interior Lighting Systems commented: “The UJA1018 enables HELLA to introduce a very compact LED ambient lighting solution that fits every interior location. The Node Position Detection by means of the integrated LIN switch allows configuration of each ambient lighting module once mounted in the car. Thus, all modules in the car can be kept the same which allows a high level of reuse and greatly simplifies the logistics.”

Pictures with Ambient Lighting application provided by Hella:

Courtesy of Hella

Availability

Samples are available.

Links

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.2 billion in 2011. Additional information can be found by visiting www.nxp.com.

How to search?