Latest videos

  • Introducing Cortex-M4 based NXP LPC4000 Series Mic...

    youtube video

    Introducing Cortex-M4 based NXP LPC4000 Series Microcontrollers


NXP Expands LPC4000 Digital Signal Controller Family

September 19, 2012

LPC408x and LPC407x based on ARM Cortex-M4 offer drop-in compatibility with popular LPC1780 and LPC1770 microcontrollers

Eindhoven, Netherlands and San Jose, California, September 19, 2012 – NXP Semiconductors N.V. (NASDAQ: NXPI) today announced the availability of its LPC408x and LPC407x microcontrollers, featuring advanced signal processing capabilities and a wide range of connectivity options, including USB 2.0, Ethernet and CAN 2.0B. Based on an ARM® Cortex™-M4 processor, the new LPC4000 microcontrollers offer drop-in compatibility with NXP’s popular LPC178x and LPC177x series, as well as multiple LPC2000 microcontrollers. The LPC408x and LPC407x are a cost-effective, low-power solution for digital signal control, ideal for displays, scanners, industrial networking, alarm systems, medical diagnostics, and motor-control applications. NXP is showcasing its latest additions to the LPC4000 family this week at DESIGN East 2012 (Booth 600), and a preview is available here: http://www.youtube.com/watch?v=_e28iZmQEj4

“The LPC408x and LPC407x series provide embedded designers with a stepping stone from our Cortex-M3 based families to our high performance dual-core LPC4300 – which at 204 MHz remains the fastest Cortex-M4 microcontroller available today,” said Gordon Cooper, international product marketing manager, microcontroller business line, NXP Semiconductors. “We are offering a clear migration path for customers already using NXP Cortex-M3 and ARM7 microcontrollers.”

Operating at speeds of up to 120 MHz, the LPC408x and LPC407x provide up to 512 KB of flash, 96 KB of SRAM, 4 KB of EEPROM, two analog comparators, and a wide range of connectivity peripherals, including up to five UARTs, three SPI/SSP, and three I2C interfaces. The LPC408x and LPC407x series feature a multi-layer AHB bus that allows high-bandwidth peripherals such as Ethernet and full-speed USB to run simultaneously, without affecting performance. Other serial peripherals include two CAN controllers, SD/MMC and an I2S interface.

Like the dual-core LPC4300 family, the LPC408x and LPC407x microcontrollers feature an optional 32-bit floating point unit, as well as a graphical LCD controller offering 1024 x 768 pixel display resolution. The new LPC microcontrollers also feature NXP’s unique SPI flash interface (SPIFI), which allows embedded system designers to add a significant amount of low-cost memory.

The LPC407x/8x devices will be available in LQFP packages with 80, 144 or 208 pins and in TFBGA packages with 180 or 208 pins. Product samples will be available from major distribution partners by the end of the month. Development boards are now available from Code Red Technologies and Embedded Artists, with additional boards to be released by IAR later this year.

Code Red RDB4078 Development Board

Featuring the NXP LPC4078 microcontroller, the Code Red RDB4078 includes a 320 x 240 IPS touchscreen with wide viewing angle, Ethernet, RS232, USB device and host, microSD, as well as advanced audio functionality including high-quality Wolfson stereo codecs and stereophonic digital microphones on board. All I/O functionality is accessible simultaneously, without the need to reconfigure the board. The RDB4078 includes on-board debug for instant debugging, taking advantage of the extensive LPC4000 support available in LPCXpresso and Red Suite. A suite of example applications, including an embedded web server, audio examples, and an SD-card filing system, is also available.

“The LPC4078 is straightforward and simple to use, delivering the DSP instructions and hardware floating point of the Cortex-M4, while feeling very familiar to NXP LPC microcontroller users,” said John Rayfield, chief executive officer, Code Red Technologies, Inc. “We’ve designed the RDB4078 development kit with the same ease of use in mind, offering a stunning display, as well as high-specification audio system features – all working out of the box.”

Links

LPC4080 and LPC4070 product information

Development boards

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.2 billion in 2011. Additional information can be found by visiting www.nxp.com.

How to search?