Latest videos

  • LPC-Link 2 Debug Adapter Extends LPCXpresso Ecosys...

    youtube video

    LPC-Link 2 Debug Adapter Extends LPCXpresso Ecosystem

NXP Extends Links to LPCXpresso Ecosystem with LPC-Link 2

April 24, 2013

Standalone debug link offers compatibility with multiple tools and IDEs

Eindhoven, Netherlands and San Jose, California, April 24, 2013 – NXP Semiconductors (NASDAQ: NXPI) today introduced LPC-Link 2 – the first standalone debug adapter of its kind, which can link a variety of popular IDEs (integrated development environments) to any microcontroller development board. The LPCXpresso-IDE, developed by Code Red Technologies, works out of the box with LPC-Link 2. In addition, several firmware images are available for LPC-Link 2 which make it compatible with other tools, including the popular SEGGER J-Link and the CMSIS-DAP debugger designed by ARM.

“LPC-Link 2 provides embedded developers with unprecedented flexibility and choice, enabling them to connect their favorite IDEs and development tools to nearly any type of board, at a very low cost,” said Henrik Flodell, tools and embedded ecosystem manager, microcontroller business line, NXP Semiconductors. “With close to 100,000 LPCXpresso boards shipped so far, we’re very excited about the introduction of LPC-Link 2 and how it will help to expand the LPCXpresso ecosystem even further.”

Firmware images of SEGGER J-Link and the CMSIS-DAP debugger can be downloaded for free from and loaded via a user-friendly DFU (device firmware update) tool. The LPC-Link2 is powered by an NXP LPC4300 series microcontroller, and includes a standard 10-pin JTAG/SWD connector; a 20-pin JTAG/SWD/ETM connector; and analog, digital and serial expansion headers, making it a highly extensible platform.

“The J-Link emulator has become a de-facto standard when it comes to debug technology for ARM processors. With more than 100,000 J-Links sold to date, its broad platform support and popularity make it an ideal companion for the LPC-Link 2 platform,” said Rolf Segger, chief technology officer of SEGGER. “The J-Link software provides exceptionally fast flash download speeds, and also allows LPC-Link 2 to be used with any major tool chain, including free GDB-based ones. It is fun to work with.”

The LPC-Link2 is available for ordering immediately from NXP as OM13054 for a recommended price of $20.00. NXP will also discuss the LPC-Link2 in a technical session at DESIGN West 2013, “Kickstarting your NXP embedded development with LPCXpresso,” which takes place on Thursday, April 25 at 11:45 am Pacific Time in booth no. 1523.


About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power Management, Interface, Security and Digital Processing expertise. These innovations are used in a wide range of automotive, identification, wireless infrastructure, lighting, industrial, mobile, consumer and computing applications. A global semiconductor company with operations in more than 25 countries, NXP posted revenue of $4.36 billion in 2012. Additional information can be found by visiting

How to search?

Already registered to MyNXP? or Register