NXP Reduces Smartphone Interference with Improved Family of Best Efficiency Audio Amplifiers

July 16, 2013

Automotive audio enhancement supports NXP’s vision of connecting the car

Eindhoven, Netherlands, July 16, 2013 – NXP Semiconductors N.V. (NASDAQ: NXPI) today announced enhancements to its industry leading family of Class-AB audio amplifiers, providing improved quiescent current reduction and decreased smart phone signal interference. The integrated GSM input filtering is built in for increased EMC robustness. Building on NXP’s expertise in Best Efficiency Mode audio applications, the TDF8546A (4x 25Watt) and TDF8548A (4x 28Watt) are also the industry’s first Class-AB amplifiers to extend line driver detection to 1kOhm load impedance.

As smartphone connectivity becomes increasingly central to automotive infotainment applications, the industry has to ensure that audio quality is not compromised by smartphone signal interference. Designed specifically for automotive applications, NXP’s Class-AB audio amplifiers provide increased GSM robustness to mitigate the influence of smartphones on loud speakers, responding to OEMs’ demand for a cost-effective solution that improves sound quality.

The TDF8546, TDF8546A and TDF8548A amplifiers are quad-channel Class-AB amplifiers available with NXP’s ground-breaking Best Efficiency Mode operating as low as 6V, reducing power dissipation by 17% compared to other high-efficiency solutions in its class. Both amplifiers enable a seamless audio experience during sudden supply voltage drops in hybrid electric vehicles and other cars using start-stop systems.

The enhancement of NXP’s family of Class-AB audio amplifiers further supports NXP’s vision of connecting the car. From telematics and car-to-x communications to smarter infotainment systems, NXP is supplying the chips making the connected car a reality. “In-car use of smart devices has become common over the past few years, but the potential interference they generate creates a major headache for audio OEMs aiming to provide excellent sound performance,” said Torsten Lehmann senior vice president and general manager car entertainment solutions at NXP Semiconductors. “These new amplifiers significantly reduce the effect that smart device signals can have on the speaker cable, while delivering superior sound performance. By improving on our best-in-class family of Class-AB audio amplifiers, NXP continues to provide robust, cost-effective, high-quality infotainment solutions to the automotive market.”


  • Four channels operating at various signal condition
  • 4 x 25W (TDF8546A) output power (14.4V, 10% THD, 4 Ohm)
  • 4 x 28W (TDF8548A) output power (14.4V, 10% THD, 4 Ohm)
  • Operating supply voltage from 6 to 18V
  • Excellent sound performance – no pop noise; suitable for 2 Ohm to 4 Ohm speakers
  • Best Efficiency Mode – low quiescent current per channel
  • Power dissipation reduced by 17% compared to other high-efficiency Class-AB amplifiers
  • Power dissipation reduced by 35% compared to standard Class-AB amplifiers
  • No switch noise due to 'soft switching'
  • Protection against short thermal overload and ESD (Electrostatic Discharge)
  • I2C bus diagnostics, including start-up diagnostics, clip detection and pre-warning
  • Small footprint: HSOP36 and DBS27 packages


About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) creates solutions that enable secure connections for a smarter world. Building on its expertise in High Performance Mixed Signal electronics, NXP is driving innovation in the automotive, identification and mobile industries, and in application areas including wireless infrastructure, lighting, healthcare, industrial, consumer tech and computing. NXP has operations in more than 25 countries, and posted revenue of $4.36 billion in 2012. Find out more at www.nxp.com.

How to search?

Already registered to MyNXP? or Register