NXP and TTTech Announce Collaboration on Automotive Ethernet Switch Chip

September 18, 2013

Eindhoven, Netherlands and Vienna, Austria, September 18, 2013 - NXP Semiconductors N.V. (NASDAQ: NXPI), the No. 1 supplier of semiconductors for automotive in-vehicle networking, and TTTech, the leading supplier of dependable networking solutions based on time-triggered technology and modular safety platforms, have signed a Memorandum of Understanding to jointly develop automotive Ethernet switch solutions supporting OPEN Alliance BroadR-Reach® Ethernet PHY technology. The switch chip will be specifically designed for the automotive market, but will also be suitable for various demanding industrial real-time applications.

NXP, with its strategic focus on the connected car, has been working with industry partners to establish BroadR-Reach as an open, de facto standard for in-vehicle Ethernet. As the first automotive semiconductor vendor to license Broadcom’s BroadR-Reach technology to develop an Ethernet PHY, NXP is taking the next step towards an integrated Ethernet switch chip in close cooperation with TTTech. Under the agreement, TTTech will provide the switch IP, while NXP implements the IP into Ethernet switch solutions with integrated PHY. The products will be ready for stringent automotive EMC, quality and reliability standards and automotive volume production.

TTTech has developed an automotive Ethernet switch IP solution based on its long-term real-time Ethernet experience in several vertical markets with high electronic robustness requirements including the aerospace, space and energy segments. TTTech’s solutions support the trend towards the demand for increasing bandwidth requirements, higher focus on reliability in networked control systems as well as high availability in fail-operational applications, like driver assistance systems. Several standards including standard Ethernet (IEEE 802.3), Time-Triggered Ethernet (SAE AS6802) as well as AVB 1.0 and the evolving TSN (Time Sensitive Network) are supported in TTTech’s chip IP.

The jointly developed switch chip will enable applications with unshielded twisted pair cabling with BroadR-Reach PHY technology. It is the first Ethernet switch chip with three incorporated traffic classes including standard Ethernet traffic for diagnostics and ECU flashing, asynchronous rate-constrained traffic for audio/video streaming and sensor fusion, as well as synchronous traffic for hard real-time control and fail-operational systems. Hence, this new automotive switch chip will enable unified Ethernet networks and the convergence of critical and non-critical application data streams on one single network.

“We look forward to working closely with TTTech, as we jointly develop an innovative automotive Ethernet switch solution,” says Toni Versluijs, VP and General Manager, In-Vehicle Networking Product Line, NXP Semiconductors. “We believe the value proposition of TTTech’s Ethernet IP together with NXP’s proven technology for the connected car will lead to compelling automotive solutions for our customers.”

“Automotive and industrial customers can now benefit from TTTech’s decade long experience with deterministic networking and TTEthernet in the new automotive switch chip solutions from NXP. We are proud to work with NXP in this strategic partnership to serve a rapidly growing market demand for standards-based deterministic Ethernet networks across multiple automotive and industrial verticals,” comments Georg Kopetz, Member of the Executive Board at TTTech.

About TTTech Computertechnik AG

TTTech Computertechnik AG is the leading supplier of dependable networking solutions based on time-triggered technology and modular safety platforms. One of the company’s core technologies is TTEthernet, a scalable, open real-time Ethernet platform used for safety-related applications. TTTech’s solutions improve the safety and reliability of networked electronic systems in the transportation and industrial segments. Our product portfolio offers best-in-class certifiable products according to IEC 61508, ISO 26262, EN 13849, DO-254 and DO-178B requirements.

TTTech customers win as they deploy dependable networks and real-time controls more efficiently and profitably. Benefits include shorter time-to-market due to re-use of proven architecture and ease of system integration with reduced cost. The company’s solutions further support highly scalable and modular open real-time architectures.

More information about TTTech is available at www.tttech.com

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) creates solutions that enable secure connections for a smarter world. Building on its expertise in High Performance Mixed Signal electronics, NXP is driving innovation in the automotive, identification and mobile industries, and in application areas including wireless infrastructure, lighting, healthcare, industrial, consumer tech and computing. NXP has operations in more than 25 countries, and posted revenue of $4.36 billion in 2012. Find out more at www.nxp.com.

Note: BroadR-Reach is a registered trademark of Broadcom Corporation. All other trademarks are property of their respective owners.

How to search?

Already registered to MyNXP? or Register