NXP Secures Over Two Billion Payment and Government ID Cards with SmartMX

September 23, 2013

SmartMX™ technology from NXP Semiconductors ensures complete identity protection

Eindhoven, Netherlands, September 23, 2013 – NXP Semiconductors N.V. (NASDAQ: NXPI) today announced that it has shipped over two billion SmartMX™ secure microcontroller chips to the growing chip-enabled payment and government identity card markets. The increasing adoption of contactless and dual interface payments cards in the financial sector and the increasing trend to issue electronic government documents means that security chips are being used more than ever to protect personal information and data.

With digital identity theft concerns at an all-time high, SmartMX technology from NXP ensures that personal information kept on banking cards, e-passports or national ID cards is always protected. Built on NXP’s IntegralSecurity™ process, SmartMX products have over 100 advanced features for attack protection and have achieved Common Criteria Evaluation Assurance Level (CC EAL) 6+ certification, one of the world’s most trusted and robust security profiles. In the never ending race to offer advanced security protection, NXP continues to innovate and incorporate the latest technology to safeguard information. Future NXP SmartMX secure microcontrollers will feature PUF (Physically Unclonable Function) technology from Intrinsic-ID. PUF safeguards individual chips from data theft by using a unique ‘fingerprint’ to protect the encryption key, therefore making the device extremely hard to clone and reverse-engineer.

“The advancements made in digital government and contactless payment cards over the years have been remarkable. For NXP, reaching the ‘two billion shipped’ milestone for our SmartMX security chips clearly demonstrates the trust institutions and governments globally place in NXP to provide convenient and secure interactions,” said Ulrich Huewels, vice president and general manager, secure card solutions, NXP Semiconductors. “These organizations offer individuals peace of mind in our increasingly complex, open and connected world. It’s imperative that we continue to develop best-in-class, innovative solutions that keep personal data safe.”

Serving banks all over the world, from Shanghai to London and New York to Berlin, NXP’s SmartMX secures transactions on over one third of the chip-based payment cards in circulation. Just over three billion chip cards are used today and in the coming years it will increase to over two billion magnetic stripe cards, currently the most widely used type of credit card, will migrate to chip-based or contactless credit cards. This aggressive migration is primarily driven by the implementation of the People’s Bank of China (PBOC) IC card standard in China and the roll out of EMV-based banking cards in the United States. In addition to security, the convenience of tap and pay offered by contactless chip cards is driving the increasing adoption of dual-interface cards. Such cards can be used in both contactless applications as well as in contact terminals like ATMs. Contactless payment cards also provide improved efficiencies in the payment process, with transaction times of less than 300ms.

NXP’s SmartMX products are also the core component in a wide variety of digital identity schemes and are deployed in close to 100 countries implementing government electronic ID programs. Used in many sovereign electronic documents such as ePassports, citizen cards, national ID cards, driving licenses, social security cards and, health cards, SmartMX-based solutions protect citizens from identity theft and reduce fraud via the products’ world class security features. Responding to the increasing pressure for effective online public administration processes and improved efficiencies, many governments consider electronic ID cards as the perfect solution, enabling citizens to securely and conveniently engage as needed. Electronic ID cards have become a prerequisite for an open and connected world where private and public businesses prosper.

About NXP Semiconductors

NXP Semiconductors N.V. (NASDAQ: NXPI) creates solutions that enable secure connections for a smarter world. Building on its expertise in High Performance Mixed Signal electronics, NXP is driving innovation in the automotive, identification and mobile industries, and in application areas including wireless infrastructure, lighting, healthcare, industrial, consumer tech and computing. NXP has operations in more than 25 countries, and posted revenue of $4.36 billion in 2012. Find out more at www.nxp.com.

How to search?

Already registered to MyNXP? or Register