Diodes
- Bandswitching diodes ( 3 )
- PIN diodes ( 44 )
- General purpose Schottky diodes ≤ 250 mA ( 91 )
- Medium power Schottky diodes ≥ 200 mA ( 158 )
- Schottky diodes (low capacitance RF) ( 13 )
- Varicap diodes
- Power diodes (hyperfast recovery) ( 25 )
- Power diodes (ultrafast recovery) ( 63 )
- Power Schottky diode ( 5 )
- Switching diodes ( 86 )
- Zener diodes ( 1344 )
A cheaper alternative to IC solutions for basic regulation functions
Common characteristics:
Please wait. Loading data...
Parametric search is unavailable at this time. Please try again later.
How to use the parametric search?
- This is the new version of the parametric search. All browsers are supported, but some functions such as the remote control and ShareThis are missing in Internet Explorer 6 and 7.
- Your feedback on the new parametric search is more than welcome. You can use the feedback button on the right of the screen to send us your feedback.
- The parametric search opens by default in a minimize version, you can use the maximize button in the right corner to use the full screen.
- You can choose the number of results per page: 10, 25, 50, 100 or all results.
- The common characteristics are parameters with the same value for all type numbers.
- You can use the filters in the second row to narrow down the selection. Click on one or more values in the lists you want to select. Or use the sliders by dragging the handlers or fill in the fields and click on Apply.
- You can find more information about a type number by hovering over the type number and click on one of the links in the pop-up.
- You can compare two or more type numbers by selection the checkboxes for the type numbers and click on Compare. All other rows will be hidden.
- To add or remove columns with parameters click on the Add/Remove Columns button. You can check de columns you want to see.
- You can change the order of the columns by dragging and dropping the columns to the desired position.
- You can download the results of your (filtered) selection to Excel by clicking the Download Excel button.
- At the bottom of the screen you can find the remote control, which you can use to scroll to the left and right, when the scrollbar is not visible.
- You can share the parametric search with others using the ShareThis option on top of the page.




Follow us