NXP Semiconductors


Select site:

English

74HC193; 74HCT193

Parametric Search

Datasheet

74HC193; 74HCT193
(Product Specification)
23-May-07, 29 pages, 150 kB

Download all documentation

General description

The 74HC193 and 74HCT193 are high-speed Si-gate CMOS devices and are pin compatible with Low power Schottky TTL (LSTTL). They are specified in compliance with JEDEC standard no. 7A.

The 74HC193 and 74HCT193 are 4-bit synchronous binary up/down counters. Separate up/down clocks, CPU and CPD respectively, simplify operation. The outputs change state synchronously with the LOW-to-HIGH transition of either clock input. If the CPU clock is pulsed while CPD is held HIGH, the device will count up. If the CPD clock is pulsed while CPU is held HIGH, the device will count down. Only one clock input can be held HIGH at any time, or erroneous operation will result. The device can be cleared at any time by the asynchronous master reset input (MR); it may also be loaded in parallel by activating the asynchronous parallel load input (PL).

The 74HC193 and 74HCT193 each contain four master-slave JK flip-flops with the necessary steering logic to provide the asynchronous reset, load, and synchronous count up and count down functions.

Each flip-flop contains JK feedback from slave to master, such that a LOW-to-HIGH transition on the CPD input will decrease the count by one, while a similar transition on the CPU input will advance the count by one.

One clock should be held HIGH while counting with the other, otherwise the circuit will either count by twos or not at all, depending on the state of the first flip-flop, which cannot toggle as long as either clock input is LOW. Applications requiring reversible operation must make the reversing decision while the activating clock is HIGH to avoid erroneous counts.

The terminal count up (TCU) and terminal count down (TCD) outputs are normally HIGH. When the circuit has reached the maximum count state of 15, the next HIGH-to-LOW transition of CPU will cause TCU to go LOW.

TCU will stay LOW until CPU goes HIGH again, duplicating the count up clock.

Likewise, the TCD output will go LOW when the circuit is in the zero state and the CPD goes LOW. The terminal count outputs can be used as the clock input signals to the next higher order circuit in a multistage counter, since they duplicate the clock waveforms. Multistage counters will not be fully synchronous, since there is a slight delay time difference added for each stage that is added.

The counter may be preset by the asynchronous parallel load capability of the circuit. Information present on the parallel data inputs (D0 to D3) is loaded into the counter and appears on the outputs (Q0 to Q3) regardless of the conditions of the clock inputs when the parallel load (PL) input is LOW. A HIGH level on the master reset (MR) input will disable the parallel load gates, override both clock inputs and set all outputs (Q0 to Q3) LOW. If one of the clock inputs is LOW during and after a reset or load operation, the next LOW-to-HIGH transition of that clock will be interpreted as a legitimate signal and will be counted.

Features

  • Synchronous reversible 4-bit binary counting
  • Asynchronous parallel load
  • Asynchronous reset
  • Expandable without external logic

Products/packages

Type numberNorth American Type numberOrdering code (12NC)Product statusPackagePackingMarkingChemical contentLeadfree conversion date
74HC193D74HC193D9337 146 20652Volume productionSOT109-1
(SO16)
Bulk Pack, CECCStandard Marking74HC193D
week 30, 2004
74HC193D74HC193D-T9337 146 20653Volume productionSOT109-1
(SO16)
Reel Pack, SMD, 13", CECCStandard Marking74HC193D
week 30, 2004
74HC193DB74HC193DB9351 886 10112Volume productionSOT338-1
(SSOP16)
TubeStandard Marking74HC193DB
week 13, 2005
74HC193DB74HC193DB-T9351 886 10118Volume productionSOT338-1
(SSOP16)
Reel Pack, SMD, 13"Standard Marking74HC193DB
week 13, 2005
74HC193N74HC193N9336 694 80652Volume productionSOT38-4
(DIP16)
Bulk Pack, CECCStandard Marking74HC193N
Always Pb-free
74HC193PW74HC193PW9351 889 80112Volume productionSOT403-1
(TSSOP16)
TubeStandard Marking74HC193PW
week 10, 2005
74HC193PW74HC193PW-T9351 889 80118Volume productionSOT403-1
(TSSOP16)
Reel Pack, SMD, 13"Standard Marking74HC193PW
week 10, 2005
74HCT193D74HCT193D9337 151 00652Volume productionSOT109-1
(SO16)
Bulk Pack, CECCStandard Marking74HCT193D
week 6, 2004
74HCT193D74HCT193D-T9337 151 00653Volume productionSOT109-1
(SO16)
Reel Pack, SMD, 13", CECCStandard Marking74HCT193D
week 6, 2004
74HCT193DB74HCT193DB9351 897 30112Volume productionSOT338-1
(SSOP16)
TubeStandard Marking74HCT193DB
week 12, 2005
74HCT193DB74HCT193DB-T9351 897 30118Volume productionSOT338-1
(SSOP16)
Reel Pack, SMD, 13"Standard Marking74HCT193DB
week 12, 2005
74HCT193N74HCT193N9336 701 10652Volume productionSOT38-4
(DIP16)
Bulk Pack, CECCStandard Marking74HCT193N
Always Pb-free
74HCT193PW74HCT193PW9352 830 88112Volume productionSOT403-1
(TSSOP16)
TubeStandard Marking74HCT193PW
Always Pb-free
74HCT193PW74HCT193PW-T9352 830 88118Volume productionSOT403-1
(TSSOP16)
Reel Pack, SMD, 13"Standard Marking74HCT193PW
Always Pb-free

Pricing/ordering/availability

Type numberOrdering code(12NC)Indicative price/unit($)RegionDistributorIn stockInventory dateBuy onlineSamples
74HC193D9337 146  20652  0.3000NAARROW ELECTRONICS169/3/2008 Buy online not available
   NADIGI-KEY CORPORATION1,3079/3/2008 Buy online  
   NAFUTURE ELECTRONICS8109/3/2008 Buy online  
74HC193D9337 146  20653  0.3000NAMOUSER ELECTRONICS2,4809/3/2008 Buy online Order samples
74HC193DB9351 886  10112  0.3400NADIGI-KEY CORPORATION9349/3/2008 Buy online not available
74HC193DB9351 886  10118  0.3400      Order samples
74HC193N9336 694  80652  0.3200NAARROW ELECTRONICS2,0509/3/2008 Buy online Order samples
   NAAVNET ELECTRONICS MARKETING1,8009/4/2008 Buy online  
   NAFUTURE ELECTRONICS1,7989/3/2008 Buy online  
74HC193PW9351 889  80112  0.3000     not available
74HC193PW9351 889  80118  0.3000      Order samples
74HCT193D9337 151  00652  0.3000NADIGI-KEY CORPORATION1,7859/3/2008 Buy online not available
   EUFARNELL1,0009/4/2008 Buy online  
   NANEWARK1,0009/4/2008 Buy online  
74HCT193D9337 151  00653  0.3000NAARROW ELECTRONICS2,5009/3/2008 Buy online Order samples
   NAMOUSER ELECTRONICS2,5009/3/2008 Buy online  
74HCT193DB9351 897  30112  0.3400NADIGI-KEY CORPORATION3679/3/2008 Buy online not available
74HCT193DB9351 897  30118  0.3400      Order samples
74HCT193N9336 701  10652  0.3400NAARROW ELECTRONICS8329/3/2008 Buy online Order samples
   EUFARNELL1,1849/4/2008 Buy online  
   NANEWARK1,1849/4/2008 Buy online  
74HCT193PW9352 830  88112       not available
74HCT193PW9352 830  88118        Order samples

Block diagrams/pinning

Technical documents

Support Documents

Parametrics/similar products

Type numberPackageDescriptionFmax(MHz)Propagation Delay(ns)VoltagePower Dissipation ConsiderationsLogic Switching LevelsOutput Drive Capability
74HC193DSOT109-1
(SO16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks 45 20@5V 2.0-6.0 V Low Power or Battery Applications CMOS +/- 5.2 mA
74HC193DBSOT338-1
(SSOP16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks 45 20@5V 2.0-6.0 V Low Power or Battery Applications CMOS +/- 5.2 mA
74HC193NSOT38-4
(DIP16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks 45 20@5V 2.0-6.0 V Low Power or Battery Applications CMOS +/- 5.2 mA
74HC193PWSOT403-1
(TSSOP16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks 45 20@5V 2.0-6.0 V Low Power or Battery Applications CMOS +/- 5.2 mA
74HCT193DSOT109-1
(SO16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks; TTL Enabled 47 20 4.5-5.5V Low Power TTL +/- 4 mA
74HCT193DBSOT338-1
(SSOP16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks; TTL Enabled 47 20 4.5-5.5V Low Power TTL +/- 4 mA
74HCT193NSOT38-4
(DIP16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks; TTL Enabled 47 20 4.5-5.5V Low Power TTL +/- 4 mA
74HCT193PWSOT403-1
(TSSOP16)
Presettable Synchronous 4-Bit Binary Up/Down Counter; Separate Up/Down Clocks; TTL Enabled 47 20 4.5-5.5V Low Power TTL +/- 4 mA

Similar products

74HC193; 74HCT193 links to the similar products page containing an overview of products that are similar in function or related to the type number(s) as listed on this page. The similar products page includes products from the same catalog tree(s), relevant selection guides and products from the same functional category.

Disclaimer

The information published on product information pages of the www.nxp.com or www.semiconductors.com websites is an extract from product data sheets and is for information purposes only. For detailed information please check the most recent version of the relevant product data sheet as published on these websites. In the event of any conflict between product information pages and data sheets or deviations from information provided in the product data sheets on these product information pages, the information provided in the product data sheets shall prevail.


The product status of the product(s) described in the product data sheet may have changed since publication of the data sheet and therefore information in datasheets on product status may be outdated. The latest information on product status is published on the product information pages of the above-mentioned websites.


As from October 1st, 2006 Philips Semiconductors has a new trade name - NXP Semiconductors, which will be used in future data sheets together with new contact details. In data sheets where the previous Philips references remain, please use the new links as shown below.


http://www.philips.semiconductors.com use http://www.nxp.com
http://www.semiconductors.philips.com use http://www.nxp.com (Internet)
sales.addresses@www.semiconductors.philips.com use salesaddresses@nxp.com (e-mail)

The copyright notice at the bottom of each page (or elsewhere in the document, depending on the version)
- © Koninklijke Philips Electronics N.V. (year). All rights reserved -
is replaced with:
- © NXP B.V. (year). All rights reserved.-


If you have any questions related to the data sheet, please contact our nearest sales office via e-mail or phone (details via salesaddresses@nxp.com). Thank you for your cooperation and understanding.