NXP Semiconductors


Select site:

English

Datasheet

HT2DC20S20
(Product Specification)
01-Oct-01, 16 pages, 68 kB

Download all documentation

General description

The HITAG (1) stick transponder HT2DC20S20 is a high performance transponder for bi-directional transmission in full-duplex between the read and write device and the transponder. Data is stored in the transponder in a non-volatile memory (EEPROM). The transponder requires no internal power supply; it derives its power from the magnetic component of the RF carrier frequency generated by the reader. Data is transmitted by modulating this carrier. The HT2DC20S20 is dedicated for use in secure access systems where the transponder and the reader have to identify each other. The choosable use of cryptography enables highest data security. Providing several operating modes (password, crypto and standard read-only modes) the versatile transponder can be used in various applications. The HALT command can be used after finishing data exchange to reach the halt state. In this state the transponder is muted. This feature can be used to have steady RF field where single transponders are collected one by one. Each transponder is operated and then disabled, so it does not interfere with the next transponder. The HALT state can only be exited by switching off and removing the magnetic field. The EEPROM has a capacity of 256 bits and is organized in 8 pages of 4 bytes. The 8 pages are split up into 4 pages containing user data and into 4 pages for control of the memory access and for authentication purposes. The pages of the transponder memory can be protected against read and write access by setting corresponding memory flags. Data transmission from the HT2DC20S20 to the reader uses Manchester or biphase coding and Amplitude Shift Keying (ASK) modulation. Absorption modulation is used to transmit data from the transponder to the reader. The transponder absorbs the magnetic field which hence modulates the current in the reader antenna. Data transmission from the reader to the HT2DC20S20 uses Binary Pulse Length Modulation (BPLM).

(1) HITAG - is a trademark of Philips Semiconductors Gratkorn GmbH.

Features

  • Identification transponder for use in contactless applications
  • Operating frequency 125 kHz
  • Data transmission and supply energy via RF link, no internal battery
  • Reading distance same as writing distance
  • Non-volatile memory of 256 bits (128 bits user data, 128 bits control data and secret memory) organized in 8 pages, 4 bytes each
  • Ten years non-volatile data retention
  • More than 100000 erase/write cycles
  • Selective read/write protection of memory content
  • Two coding schemes for read operation: biphase and Manchester coding
  • Effective communication protocol with outstanding data integrity check
  • Mutual authentication function
  • Read/write mode allows:
    • Plain data transmission (password check)
    • Encrypted data transmission (crypto mode).
  • In read/write mode multi-tag operation possible because of special HALT function
  • Emulation of standard industrial read-only transponders:
    • Public mode A (64 bits read-only)
    • Public mode B (according to ISO 11785 for animal identification)
    • Public mode C (PIT compatible mode).
  • Special features:
    • User defined write protection
    • Unique 32-bit serial number for each transponder
    • Read-only emulation function
    • Encrypted data transmission possible.


Products/packages

Type numberNorth American Type numberOrdering code (12NC)Product statusPackagePackingMarkingChemical contentLeadfree conversion date
HT2DC20S20/FHT2DC20S20M9352 339 40122Volume productionSOT385-1
(PLLMC)
Stick and CoinsStandard MarkingHT2DC20S20/F
Always Pb-free

Pricing/ordering/availability

Type numberOrdering code(12NC)Indicative price/unit($)RegionDistributorIn stockInventory dateBuy onlineSamples
HT2DC20S20/F9352 339  40122  NADIGI-KEY CORPORATION5,54410/11/2008 Buy online Order samples
   NAMOUSER ELECTRONICS4,97910/10/2008 Buy online  

Applications

  • Optimized as a control FET in DC to DC converters.


Disclaimer

The information published on product information pages of the www.nxp.com or www.semiconductors.com websites is an extract from product data sheets and is for information purposes only. For detailed information please check the most recent version of the relevant product data sheet as published on these websites. In the event of any conflict between product information pages and data sheets or deviations from information provided in the product data sheets on these product information pages, the information provided in the product data sheets shall prevail.


The product status of the product(s) described in the product data sheet may have changed since publication of the data sheet and therefore information in datasheets on product status may be outdated. The latest information on product status is published on the product information pages of the above-mentioned websites.


As from October 1st, 2006 Philips Semiconductors has a new trade name - NXP Semiconductors, which will be used in future data sheets together with new contact details. In data sheets where the previous Philips references remain, please use the new links as shown below.


http://www.philips.semiconductors.com use http://www.nxp.com
http://www.semiconductors.philips.com use http://www.nxp.com (Internet)
sales.addresses@www.semiconductors.philips.com use salesaddresses@nxp.com (e-mail)

The copyright notice at the bottom of each page (or elsewhere in the document, depending on the version)
- © Koninklijke Philips Electronics N.V. (year). All rights reserved -
is replaced with:
- © NXP B.V. (year). All rights reserved.-


If you have any questions related to the data sheet, please contact our nearest sales office via e-mail or phone (details via salesaddresses@nxp.com). Thank you for your cooperation and understanding.