The PCF87852 combines the BluetoothTM protocol stack, Link Controller (LC), Link Manager (LM), and Host Controller Interface (HCI) firmware of the Bluetooth system specification in a single IC with embedded software. Together with an RF module, a few external components and an antenna it forms a Bluetooth system. In most cases this module will be attached to a host, for example a GSM baseband controller or a PC processor. The PCF87852 may also be used for embedded Bluetooth applications by running the upper software layers also from the on-chip memory. Together with an external voice codec a Bluetooth headset application can be realized.
The industry standard ARM7TDMITM microcontroller with low power consumption is integrated together with ROM memory and SRAM. There are no provisions for external controllers to directly access on-chip data memory. Communication with an external host, for example a PC, GSM or PDA, is handled via the HCI.
Industry standard interfaces such as I2C-busTM, PCM and IOM® are supported by on-chip hardware. Additionally, a UART interface is available that can be used as the Bluetooth host controller interface.
The Bluetooth controller consists of a number of functional blocks that operate under control of the embedded microcontroller. The microcontroller has access to these blocks via the AMBA System Bus (ASB) and the VLSI Peripheral Bus (VPB).
The PCF87852 is designed to be used together with an RF IC as low-cost, low-power, radio-based cable replacement or wireless link. This link will be the basis for PCs, telephones, PDAs and peripherals to communicate together on an ad-hoc basis. It will replace cables and enables a wireless personal network.
The PCF87852 is especially suited for applications without the need for analog voice input or output, e.g. cellular telephones or computing platforms.
The information published on product information pages of the www.nxp.com or www.semiconductors.com websites is an extract from product data sheets and is for information purposes only. For detailed information please check the most recent version of the relevant product data sheet as published on these websites. In the event of any conflict between product information pages and data sheets or deviations from information provided in the product data sheets on these product information pages, the information provided in the product data sheets shall prevail.
The product status of the product(s) described in the product data sheet may have changed since publication of the data sheet and therefore information in datasheets on product status may be outdated. The latest information on product status is published on the product information pages of the above-mentioned websites.
As from October 1st, 2006 Philips Semiconductors has a new trade name - NXP Semiconductors, which will be used in future data sheets together with new contact details. In data sheets where the previous Philips references remain, please use the new links as shown below.
The copyright notice at the bottom of each page (or elsewhere in the document, depending on the version)
- © Koninklijke Philips Electronics N.V. (year). All rights reserved -
is replaced with:
- © NXP B.V. (year). All rights reserved.-
If you have any questions related to the data sheet, please contact our nearest sales office via e-mail or phone (details via salesaddresses@nxp.com). Thank you for your cooperation and understanding.