NXP Semiconductors


Select site:

English

UBA3070

Selection guide

Datasheet

UBA3070
(Product Specification)
02-Dec-08, 13 pages, 78 kB

Download all documentation

General description

The UBA3070 driver IC is the first member of a first generation of power-efficient LED backlight driver ICs.

Highly efficient, flexible and reliable LED drivers can easily be designed using the UBA3070 control IC.

Features

  • Switch-mode buck controller that drives strings of LEDs up to 600 V power-efficiently
  • Controller with power-efficient boundary conduction mode of operation:
    • No reverse recovery losses in freewheel diode
    • Zero current switching for turn-on of switch
    • Zero voltage or valley switching for turn-on of switch
    • Minimal required inductance value and size
  • Direct Pulse Width Modulation (PWM) dimming available
  • Fast transient response through cycle-by-cycle current control, thereby:
    • Preventing over or undershoots in the LED current
    • Enabling efficient PWM dimming by quickly turning the converter on and off and thereby removing the need for extra dim switches and high-side drivers
  • Single loosely controlled input voltage required for all LED strings in RGB backlights
  • No binning on LED forward voltage required
  • Protections:
    • Undervoltage lockout
    • Leading edge blanking
    • Overcurrent
    • Overtemperature
  • Low cost LED driver solution:
    • No Schottky diode required because of zero-current switching
    • No dim switch and high-side driver required for PWM dimming
    • Smaller inductor possible compared to fixed-frequency continuous conduction mode controllers

Products/packages

Type numberOrderable part numberOrdering code (12NC)Product statusPackagePackingMarkingChemical contentLeadfree conversion date
UBA3070T/N1UBA3070T/N1,1189352 856 92118Volume productionSOT96-1
(SO8)
Tape reel smdStandard MarkingUBA3070T/N1
Always Pb-free

Pricing/ordering/availability

Type numberOrdering code(12NC)Orderable part numberIndicative price/unit($)RegionDistributorIn stockOrder quantityInventory dateBuy onlineSamples
UBA3070T/N19352 856 92118  UBA3070T/N1,118  NAAVNET ELECTRONICS MARKETING10,000 7/2/2009Buy onlinenot available

Applications

  • The UBA3070 is typically suited as a high voltage LED backlighting application in LCD televisions and monitors (See Figure 1)

Block diagrams/pinning

Disclaimer

The information published on product information pages of the www.nxp.com or www.semiconductors.com websites is an extract from product data sheets and is for information purposes only. For detailed information please check the most recent version of the relevant product data sheet as published on these websites. In the event of any conflict between product information pages and data sheets or deviations from information provided in the product data sheets on these product information pages, the information provided in the product data sheets shall prevail.


The product status of the product(s) described in the product data sheet may have changed since publication of the data sheet and therefore information in datasheets on product status may be outdated. The latest information on product status is published on the product information pages of the above-mentioned websites.


As from October 1st, 2006 Philips Semiconductors has a new trade name - NXP Semiconductors, which will be used in future data sheets together with new contact details. In data sheets where the previous Philips references remain, please use the new links as shown below.


http://www.philips.semiconductors.com use http://www.nxp.com
http://www.semiconductors.philips.com use http://www.nxp.com (Internet)
sales.addresses@www.semiconductors.philips.com use salesaddresses@nxp.com (e-mail)

The copyright notice at the bottom of each page (or elsewhere in the document, depending on the version)
- © Koninklijke Philips Electronics N.V. (year). All rights reserved -
is replaced with:
- © NXP B.V. (year). All rights reserved.-


If you have any questions related to the data sheet, please contact our nearest sales office via e-mail or phone (details via salesaddresses@nxp.com). Thank you for your cooperation and understanding.