Design documents
Now select a document type to show the list of documents.
- Application notes
- Datasheets
- User manuals
- Literature
- Models
| Filename | Description | Type | Size (kb) | Date |
|---|---|---|---|---|
| AN10587 | Interfacing NXP bridge IC with... | Application note | 65 | 2007-02-26 |
| AN10571 | Sleep programming for NXP brid... | Application note | 42 | 2007-01-08 |
| AN10417 | SC16IS760/762 Fast IrDA mode | Application note | 42 | 2006-06-08 |
| AN10486 | Automatic RS-485 address detec... | Application note | 33 | 2006-06-02 |
| AN10485 | SDA pin connection in SPI mode | Application note | 33 | 2006-06-02 |
| AN10462 | SPI programming for Philips Br... | Application note | 51 | 2006-06-01 |
| AN10452 | Interfacing Philips Bridge IC ... | Application note | 72 | 2006-05-17 |
| AN10428 | UART-SPI Gateway for Philips S... | Application note | 84 | 2006-03-06 |
| AN10397 | How to use the SC18IM700 to co... | Application note | 75 | 2005-12-05 |




Follow us