EINDHOVEN,
"We are excited to sample the industry's first secure total USB Type-C solution, allowing for the seamless connectivity of data, video, security and power delivery over a single connector," said
USB Type-C connectors are expected to become the new standard in device-to-device connectivity as they grow in popularity. Offering up to 10Gbps data rates and 100 watts of power, the USB Type-C connector and cable technology supports the growing demands of computing, mobile, and consumer products.
Improving upon the previous Type-A and Type-B USB connectors, the Type-C connector is far more user-friendly, offering reversible plug orientation, cable direction and the ability to transfer power and data simultaneously as well as support different protocols, such as DisplayPort, MHL, and Thunderbolt for alternate modes. The bi-directional power flow support allows a device to either source or sink power. In addition, Type-C connectors offer scalable power solutions, ranging from 5.0 volts at 0.5 amps for handheld devices up to 20 volts at 5.0 amps for rapid charging and power delivery.
The total USB Type-C ecosystem from NXP includes microcontrollers, high speed switches, USB3 redrivers, ESD protection and filtering devices, USB PD PHY, CC logic controllers, authentication, load switches, AC/DC power solutions, MOSFETs and more. More Type-C products will be released each month. To request samples or learn more about our USB Type-C total solution, please visit www.nxp.com/usb-type-c.
About
Forward-looking statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
CONTACT: For further press information, please contact:Europe :Martijn van der Linden +31 6 10914896 martijn.van.der.linden@nxp.comGreater China /Asia :Esther Chang +886 2 8170 9990 esther.chang@nxp.comAmericas :Hillary Cain +1 408 518 5227 hillary.cain@nxp.com