Single-chip, dual-core MCU supports Bluetooth 5, Thread and Zigbee while increasing security for consumer and industrial IoT devices
NUREMBERG, GERMANY (Embedded World 2018) – February 27, 2018 – Many devices today require a host microcontroller (MCU) connected to a radio which increases size and complexity, while also making design, software development, procurement, supply planning and logistics more complex. Part of NXP’s broad edge computing portfolio, which allows devices to be more powerful and secure, is the new K32W0x wireless MCU platform – representing the next-generation of Kinetis MCUs. The K32W0x platform bridges its predecessor parts by providing a scalable path with higher performance, added functionality and increased security to address the evolving IoT landscape. This new platform is the first single chip device with a dual core architecture and embedded multi-protocol radio giving IoT product developers a single supplier for silicon, software, enablement, support and procurement reducing product complexity, size and costs – all while increasing functionality and security.
More secure IoT devices
Many IoT devices today do not have the necessary level of security to protect against threats that compromise networks. Protecting against these evolving threats is a primary focus of the K32W0x platform – designed to assure confidentiality, integrity, and authenticity of the IoT device and its data.
Security features of the K32W0x’s security system include:
To extend the on-chip security features of the K32W0x MCU platform, NXP has collaborated with B-Secur, a leader in biometric authentication, to develop a system that uses an individual’s unique heart pattern (electrocardiogram/ECG) to validate identity, making systems more secure than using an individual’s fingerprint or voice. A full demonstration of this innovative technology will be shown at Embedded World 2018 in the NXP booth 4A-220.
Device Name | Bluetooth 5 | Thread | Zigbee 3.0 |
K32W042 | √ | √ | √ |
K32W032 | √ |
|
|
K32W022 |
| √ | √ |
The K32W0x platform is sampling now and is planned to launch in late Q3. Please contact your local NXP salesperson for additional details. Learn more about the K32W0x MCU platform at www.nxp.com/K32W0x.
See NXP’s Edge Computing Solutions at Embedded World 2018
NXP will showcase its latest solutions for intelligent end-nodes, connected cars, and industrial systems at Embedded World 2018 at the NXP booth, #4A-220. A highlight for the show will be the NXP IoT Edge Compute Experience, located at the entrance to the exhibition hall 4A.
To RSVP your personalized visit to the IoT Edge Compute Experience or schedule a meeting during Embedded World 2018, please contact pr@nxp.com.
To hear the latest news for NXP at the show visit the NXP Embedded World 2018 press room.