The AFV10700H is based on NXP’s leading-edge Airfast technology and is contained in a small NI-780 air cavity package, which occupies 40 percent less space than the standard NI-1230 package used by other LDMOS solutions of similar power level today. Its highly integrated on-chip pre-matching delivers a high output impedance that helps reduce the size of the matching circuitry, enabling a 1.3″ x 2.6″ (3.3 x 6.6 cm) power amplifier. Simultaneously, the industry-leading thermal resistance further reduces the weight of the transponder by enabling smaller heatsink designs.
“This new solution is an excellent example of NXP’s commitment to develop compelling products that address the stringent requirements in size and performance of L-Band pulsed applications,” said
Designed for pulsed applications such as commercial automatic dependent surveillance — broadcast (ADS-B), UAVs and military identification, friend or foe (IFF), the device outputs 700 W P1dB at 1090 megahertz (MHz) with 50 volts (V) and 56 percent efficiency. If operated at 52 V, it can achieve 850 W P1dB at 1030 MHz with 52 percent efficiency. The low thermal impedance supports high duty factor pulse trains, such as Mode-S Extended Length Message (ELM) and Link 16.
The new offering further densifies NXP’s portfolio of 960-1215 MHz LDMOS transistors for avionics applications, which now comprises 10 different power levels from 10-1300 W. This wide offering provides RF designers with flexibility and options for their transponder designs.
Availability and Showcase
The AFV10700H transistor is in production now and is supported by a reference circuit for 1030-1090 MHz narrowband operations. For more information, visit www.nxp.com/AFV10700H.
NXP is showcasing the new transistor at the International Microwave Symposium, June 6–8, in
About
For more information, please contact:Americas Jacey ZunigaTel : +1 512-895-7398Email: jacey.zuniga@nxp.comEurope Martijn van der Linden Tel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China /AsiaEsther Chang Tel: +886 2 8170 9990Email: esther.chang@nxp.com