NXP’s Modular IoT Framework drastically reduces time, effort and expertise required to build production IoT systems versus traditional approach of assembling and integrating individual hardware and software componentsNUREMBERG, Germany, March 14, 2017 (GLOBE NEWSWIRE) -- (Embedded World 2017) -- Robust wireless connectivity, security, and associated expertise is critical to the development of any successful commercial production IoT system. NXP Semiconductors N.V. (NASDAQ:NXPI) is announcing the Modular IoT Framework that offers professional development teams a head start in building innovative and secure IoT applications. Using the framework as a starting point, versus building a platform from individual components, can save time and expense by minimizing the scope and complexity involved with the integration of security and connectivity.
The Modular IoT Framework offers flexibility to mix and match NXP’s embedded hardware and software technologies spanning the vast array of capabilities required to develop and deploy interoperable IoT systems with edge devices, gateways, connectivity, security, and commissioning. Framework components are tested and verified for ZigBee® and Thread connectivity, as well as cloud communications through Wi-Fi, Ethernet, cellular and LoRa™, enabling access to Amazon Web Services (AWS) and other cloud platform services.
“The NXP Modular IoT Framework gives Rigado the ability to quickly define, integrate, and iterate the IoT system features required by our customers via a production ready IoT platform with documented interfaces and pre-integrated connectivity and security,” said Ben Corrado, CEO of Rigado. “With many of our IoT customers focused on reducing risk and time to market, the NXP framework enables us to quickly iterate and get the right mix of industry leading hardware, software and connectivity capabilities to commercial production before our competitors.”
Today, developers can access the initial implementation of the framework as an Integrated Development Experience defined by targeted IoT use cases which includes a commercial-ready wireless connected platform, plus all of the necessary components, documentation and support required to be up and running with a base level securely connected production platform in minutes. By pre-integrating these capabilities into comprehensive, compatible, developer-ready Integrated Development Experiences, NXP is equipped to drive rapid time to market for IoT installations in smart cities, smart industries, agriculture and oil and gas markets.
“With global agriculture struggling to continue feeding the world’s population and smart agriculture presenting a unique set of environmentally sustainable solutions, we knew we wanted to act quickly and decisively,” said Jay Carlson, CTO at Solvz, manufacturer of internet-connected precision agriculture products. “The NXP IoT framework and advanced edge devices bring a welcomed advantage when developing internet-connected products; by having a vast majority of the middleware and even application software in place, we can bring products to market much faster than using traditional development patterns. This is vital as the 2017 growing seasons rapidly approach.”
“There has been a heavy emphasis in the market on bringing up extended cloud capabilities to support the growth of the IoT, but there is still a significant void when it comes to expertise required for developing the security, wireless connectivity and commissioning infrastructure required to get the plethora of IoT edge devices connected to the cloud,” said Denis Cabrol, senior director for solutions at NXP. “Acquiring proficiency in these areas can take years and integrating appropriate security and connectivity can add years of development time. NXP’s proven Modular IoT Framework drastically accelerate time to market by reducing the effort, time and expertise required to develop and connect the embedded side of fully functional and secure IoT systems.”
The framework is shipping today via an Integrated Development Experience targeting commercial lighting and building automation use cases which includes:
- Modular edge node platform with Thread and ZigBee support
- Modular IoT Gateway with support for Thread and ZigBee, Wi-Fi and Ethernet, and a secure element
- NFC based device commissioning
- Smart phone app reference design for device control via cloud
- Cloud service reference design on Amazon Web Services, and cloud connectivity reference design using MQTT and CoAP
The Integrated Development Experience is designed for ease of use and supported with documentation and a dedicated community. NXP professional support and services are also available under contract for deeper design support. For more information, visit the Modular IoT Framework Community: https://community.nxp.com/groups/modular-framework
See NXP Technologies in action at Embedded World 2017 in Nuremberg, Germany
Visit NXP during Embedded World in Hall 4A – 220 at the Exhibition Centre Nuremberg. Interact with innovative demonstrations for embedded solutions enabling the IoT from smart cars to smart industry.
For more information about NXP news at Embedded World, please visit www.nxp.com/EW17/mediacenter.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 31,000 employees in more than 33 countries and posted revenue of $9.5 billion in 2016. Find out more at www.nxp.com.
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2017 NXP B.V.
For more information, please contact:AmericasTate TranTel: +1 408-802-0602Email: tate.tran@nxp.comEuropeMartijn van der LindenTel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China / AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chang@nxp.com
NXP Semiconductors Netherlands B.V.