With increasing regulatory restrictions on emissions and stricter fuel economy targets around the world, both traditional automakers and new market entrants are under pressure to roll out electric and hybrid vehicles to consumers quickly. GreenBox provides a high-performance processing platform to design and test new control algorithms and energy management tasks critical for next-generation hybrid and fully-electric vehicles.
GreenBox is one of the development platforms for NXP’s next generation S32 electrification MCUs, which are part of the S32 automotive processing platform that is built around a safe, secure and fault-tolerant configuration. The S32 electrification MCUs will address the increasingly intensive computation and memory requirements for tomorrow’s HEV/EV applications.
Using the GreenBox development environment, developers can also tap into the mix of high-performance and highly optimized peripherals, including advanced timers, motor control peripherals and analog sub-systems to interface with their own development hardware.
GreenBox is available in two configurations. The first is for development of fully-electric vehicles and supports motor control and battery management capabilities. The second is for development of hybrid applications, which supports both electric vehicle features as well as traditional engine control capabilities.
Recently,
“The combination of regulatory and market indicators as well as long automotive development cycles require automakers to begin the development of HEV/EV systems now -- before the next wave of processors for electrification are available,”
About the GreenBox Vehicle Electrification Development Platform
NXP GreenBox at Embedded World 2018
NXP Green Box development platform will demo the performance capabilities of next-gen MCUs as they manage both the electric motor and internal combustion engine applications for the hybrid electric vehicles of tomorrow.
NXP GreenBox Is Now Available
GreenBox electrification development platform is available today in limited quantities to Alpha customers. Contact your sales person for more information.
More at www.nxp.com/GreenBox
About
For more information, please contact:
Tel: +44 7715228414
Email: jason.deal@nxp.com
Tel: +866 2 8170 9990
Email: esther.chang@nxp.com
Tel: +81-70-3627-6472
Email: kiyomi.masuda@nxp.com
Tags: Automotive