The Connectivity Standards Alliance (CSA) has released Matter 1.4.2, taking an important milestone in the evolution of the Matter standard. This update
focuses on improving security, scalability and overall user experience, including notable additions like Wi-Fi commissioning. These new features aim to
make the smart home more efficient and intuitive.
Since Matter's initial release in November 2022, the CSA
has continued to strengthen and progress toward enabling reliable and
simple-to-use smart homes. Matter 1.4.2—the latest release—enhances security
and scalability with several enhancements that are briefly summarized in the table below.
| Feature |
Description |
| Wi-Fi Only Commissioning |
Enables simple setup with Wi-Fi for when Bluetooth LE is not needed for other
functions
|
| Advanced Security Enhancements |
Provides vendor ID verification, Access Restriction Lists (ARLs), Certificate
Revocation Lists (CRLs)
|
| Improved Scenes Management |
Standardized the way controllers define and activate scenes across
multiple Matter devices
|
| Efficient Network Communication (Quieter Reporting) |
Optimizes the data model that defines when and how often devices
should report attribute changes to reduce network utilization and
extend battery life
|
| Standardized Node Reconfiguration |
Provides the method that enables for new features to become available automatically
|
| Consistent Endpoint Unique IDs |
Ensures that each endpoint has a persistent, admin-independent identifier
to remove duplicate devices or confusion when devices are reconfigured
or when their Matter connection is updated
|
| Standardized Robot Vacuum Cleaner (RVC) Behaviors |
Standardizes expected behavior, particularly around sequential
commands, for more predictable and reliable vacuum performance
|
| Enhanced Network Infrastructure Requirements |
Updates the requirements for Network Infrastructure Managers (NIMs) like
routers and access points on devices that must be supported
with Thread Border Routers and Wi-Fi Access Points
|
| Improved Certification Processes |
Updates test plans, scripts and tools that enhance test automation,
minimize ambiguity and streamline certification processes
|
One key enhancement of the latest release—Wi-Fi commissioning—is a new feature for Matter. Previously,
Matter devices had only one option to commission devices onto the
Matter network—Bluetooth Low Energy (LE). While this works well for many
device types, it does present a challenge for device types when Bluetooth LE
is not needed for the application itself, creating additional cost and
complexity. For example, large appliances such as laundry washers and dryers
may already have Wi-Fi implemented to connect to the Internet, but they do not
have compelling use cases for Bluetooth LE. It also gives device makers a way
to bring new capabilities to their Wi-Fi-only home devices by deploying Matter through a simple firmware update.
This demo showcases Matter 1.4.2 and its new support for Wi-Fi-only
commissioning, reducing cost and complexity for device applications that do not need Bluetooth LE.
The CSA Matter Working Group and the Wi-Fi Alliance collaborated to provide a solution for these types of use cases and requirements for enabling Matter devices to be on-boarded using Wi-Fi. Wi-Fi has a new feature called Unsynchronized Service Discovery that uses a lightweight
device-to-device service discovery and message exchanges without relying on
device synchronization.
Through NXP's complete Matter portfolio, we provide implementations that support
Thread, Wi-Fi or Ethernet with our Tri-Radio solutions, such as the
RW612 Wireless microcontroller unit (MCU)
(or IW612) and
IW610
system on chip (SoC), as well as our
MCX W Wireless MCUs
that address the variety of device types and use cases that Matter encompasses.
As Matter has continued to expand, support for devices, we identified the
need for this capability especially in devices that typically use only Wi-Fi
such as appliances. In collaboration with the CSA and Wi-Fi Alliance, the NXP
team contributed resources for developing Wi-Fi commissioning, and through a demo of this feature, we have seen positive feedback from the market.
Explore NXP's many solutions for the complete Matter ecosystem.
Learn more and get started on your Matter product development journey at
NXP Matter.
See the table below for a snapshot of the Matter platforms offered by NXP: