Corporate Environment Health & Safety
For more information, please contact Corporate Environment Health & Safety.
Technical content and expertise to help jump start your design and get you to production faster.
Start your designDownload our latest development and embedded software solutions.
Expedite time-to-market with our extensive lineup of development kits.
Jump-start your design with proven hardware and software solutions.
Get the latest specifications in our technical documentation library.
Further your technical expertise with online and in-person instruction.
Get comprehensive paid support to fast-track your product development.
Design ideas, demo videos, quality answers. Connect with NXP professionals and other knowledgeable designers ready to help.
Software, documentation, evaluation tools. The resources to build comprehensive solutions and accelerate your time to market.
Access our design resource libraryWe're always looking for passionate and talented people to work with us.
Join our teamIncluding Greenhouse Gases
Reducing NXP’s carbon footprint are initiatives that can make our world a better place. Regarding our operations, there are operational controls that we can make improvements to be a more responsible corporate citizen. Reducing our carbon footprint has been identified as a salient issue that our company can address and improve upon. We have company initiatives that focus on the effects of our operations and how it impacts the environment at large.
Semiconductor manufacturing is not considered a major contributor to global warming, but our operations do directly and indirectly emit greenhouse gases such as PFC’s and emissions from purchasing electricity. We measure, manage and report our Scope 1, 2 and some Scope 3 emissions. Emissions are reported in terms of tons of CO2 equivalents.
NXP’s 2020 goal is to reduce our normalized carbon footprint by 30% from a baseline year of 2010. In addition, NXP strives to aggressively reduce our “absolute” emissions, meaning a reduction regardless of the expended growth of production. Our production normalizer is based on the square meter of silicon wafers produced.
NXP aims to reduce our carbon footprint, through utility consumption conservation, process optimization, greenhouse gas replacement, point of use abatement projects, optimizing product transport and business travel. As part of this effort, our combined sites had multiple reduction projects such as:
Between 2010 and 2019, our normalized total emissions for Scope 1, 2 and 3 (direct and indirect) decreased by approximately 24% and our total absolute emissions reduced by 18%. Our normalized Scope 1, 2 and 3 emissions increased slightly from last year due to the reduction of products produced, our denominator of the normalized calculations. However, our total absolute emissions have steadily decreased resulting from the many projects over the past 9 years.
Our Scope 1 Emissions include fossil fuel (e.g. to heat buildings and the use in generators), the six Kyoto gases: CO2, CH4, N2O and SF6, including PFCs in our manufacturing of integrated circuits, and the use of HTFs, such as HydroFluoroCarbons (HFCs) and Perfluoro Ethers for device testing and cooling purposes. Our Scope 2 emissions include electricity purchased. Our Scope 3 emissions include business travel and product transport.
In 2019 our normalized Scope 1 emissions decreased by 32.5% from a 2010 baseline.
Fossil fuels are hydrocarbons, primarily coal, fuel, oil or natural gas. The burning of fossil fuels by humans is the largest source of CO2 emissions. Fossil fuels are still the main source of energy in the global economy.
At NXP, the most commonly used fossil fuel is natural gas, used for heating and humidity control in our clean rooms. NXP’s use of natural gas depends strongly on both the external temperature and internal production activity within the manufacturing facilities. Diesel is also used at NXP for back-up generators.
From 2010 to 2019, our normalized fossil fuel emissions decreased by more than 23%. Our normalized and total fossil fuel emissions increased from 2018 due to an increase in consumption and the reduction of products manufactured.
The natural gas increase occurred at one site because they increased their square footage by 30%. Additionally, three sites purchased more natural gas due to the cyclic nature of climate changing year upon year for heating requirements. We report diesel based on the purchase record. Diesel is primarily used for our emergency generators (primarily consumed for testing purposes) and forklifts. The purchase of diesel is not distributed evenly throughout the years in which there was an increased shift of purchasing from 2018 to 2019.
PFCs are essential chemicals in today’s semiconductor manufacturing processes. When it comes to etching integrated circuitry onto silicon wafers, or cleaning the internal chambers of deposition equipment, there are no alternatives for PFCs. Without them, semiconductor companies would not be able to produce the complex, high performance ICs that have become so essential to our daily lives. Nevertheless, PFCs pose a serious dilemma for every semiconductor company. We have essentially exhausted the two most cost-effective options for PFC reduction–process optimization and switching to alternative gases.
We recognize the undesirable impact PFCs have on the environment and have joined with others in the semiconductor industry to seek ways to minimize their use and emissions. For example, NXP signed the Memorandum of Understanding in the US and the Memorandum of Agreement in Europe, to voluntarily reduce the emissions of PFCs. The industry achieved this target before the 2010 deadline. The European Union has recognized the semiconductor industry’s proactive approach by granting an exemption to the so-called F-gases regulation. It is a voluntary agreement. No ban on the use of PFCs for critical applications has been imposed on the semiconductor industry in Europe. We are, however, committed to looking for alternatives.
Like the rest of the semiconductor industry, NXP Semiconductors remains strongly devoted to its proactive management of PFC emissions. We support the New 2010-2020 Global Semiconductor Industry Voluntary Agreement, including the Best Practice Guidance which addresses worldwide emissions from semiconductor manufacturing for the present decade. The agreement is supported by all members of the World Semiconductor Council (WSC) and covers the optimization of production processes (so they consume less greenhouse gases), the replacement of greenhouse gases with global warming potential (GWP)-free or lower-GWP alternatives and use of the most up-to-date abatement technology.
NXP also has its own goals for the reduction of PFC emissions. We proactively review Point-Of-Use (POU) abatement when we maintain, replace or relocate existing fab tools. As we upgrade existing process tools, we add POU abatement, when feasible. If such POU abatement is not feasible, we look for measures elsewhere in our factories to compensate for the emissions. In 2019, the Chandler fab installed 4 abatement equipment to further reduce the emissions of PFCs (NF3, CF4, C2F6).
As a global company, we use the Intergovernmental Panel on Climate Change (IPCC) for calculating our PFC emissions using the Tier 2b methodology. From 2010 to 2019, our normalized total PFC emissions decreased by 52%, even though many of our products have become more complex, requiring additional manufacturing steps and hence more PFCs.
NXP uses HTFs for device testing, for cooling purposes (manufacturing tools, facilities, and air-conditioning), and in a few cases as a fire suppressant.
During the manufacture of semiconductor devices, HTFs serve as coolants in chillers, removing excess heat during many manufacturing processes. During semiconductor device testing, devices are immersed in containers of HTFs, cooled or heated to a desired temperature to verify their integrity and exposed to HTFs to prevent overheating during certain tests. HTFs are also used to attach semiconductor devices to circuit boards via solder, which may be melted by the vapor of an HTF heated to its boiling point.
Some of the HTFs we use are ozone-depleting substances and, as such, are strictly controlled. For instance, the European Union has adopted regulation EC No 1005/2009 on substances that deplete the ozone layer. By order of this regulation, the so-called “controlled substances” are to be phased out. The phase-out date differs from country to country. NXP has strict rules in place, regarding all ozone-depleting substances, calling for their phase-out well before legislation comes into effect.
From 2013 to 2019 our normalized and total HTF emissions increased due to the higher demand of products that require HTFs for device testing.
In Action: Aligning with the 2020 goal, the Kuala Lumpur site committed to reduce Heat Transfer Fluid (HTF) emissions which is used for testing hermetically sealed RF products.
HTFs are used to detect pin hole leaks on RF power amplifiers. However, during the testing there are two steps within the testing procedure that releases HTFs into the atmosphere which are due to vapor diffusive loss and fluid drag out. HTFs contribute to one of the highest emissions of GHG from the Kuala Lumpur site.
To address HTF emission reduction at Kuala Lumpur, a three-phase project was developed. The first phase was to substitute a high global warming potential HTF with a lower global warming potential HTF. This substitution of materials reduced the emissions by 10%. The second phase modified the existing process by minimizing the surface area of the testing tray to capture more fluid in the vat and reduce the drag out which resulted in another 20% reduction of emissions. The third phase is modifying the manual system by designing a semi-automated, closed loop system. This new system will add additional mechanisms to create 2 zones in which emissions are now collected instead of emitted. The first zone captures the vaporized solvent through the cooling process and the second zone recycles the solvent in a closed loop system by condensation. This will provide an additional 40% emission reduction.
N2O is used in semiconductor processes, such as the chemical vapor deposition of silicon dioxide, doped or undoped silicon oxynitride, diffusion, rapid thermal processing and chamber seasoning.
Emissions from N2O are minor compared to other emissions such as those from PFCs. From 2010 to 2019 the normalized N2O emission decreased by 35.6%.
Additional emissions are nitrogen oxides (NOx), sulphur oxides (SOx) and volatile organic compounds (VOC). NOx and SOx are air pollutants that arise from a wide variety of sources but mainly because of combustion. NOx is a term used to refer to nitric oxide (NO) and nitrogen dioxide (NO2). SOx refer to sulphur dioxide (SO2).
At NXP, predominate NOx and SOx emissions are from the manufacturing processes of integrated circuits. Minimal NOx and SOx emissions come from our boilers. VOC emissions result from use of chemicals such as solvents used in the photolithography manufacturing process. VOCs include isopropyl alcohol (IPA) and other solvents.
From 2010 to 2019, the following normalized emission percentages for NOx, SOx and VOC are as follows: NOx decreased by 11%, SOx decreased by 66% and VOC decreased by 27%.
Our Scope 2 emissions is a result of our consumption of electricity. The indirect CO2 emission for electricity results from the combustion of fossil fuel in third-party power plants.
The CO2 conversion factor is defined as the standardized figure used within NXP to calculate the average amount of CO2 emissions, resulting from the use of energy sources. These conversion factors are country-specific and are based on information made available by the International Energy Agency.
The use of electricity and our approach to saving energy is reported in the “Energy” section.
NXP’s Scope 2 emissions are reported for electricity purchased. From 2010 to 2019, the normalized Scope 2 emissions decreased by 16%. The 2019 we had a reduction of semiconductor production. Due to the nature of the manufacturing processes and the factories not being able to adjust to lower production volumes, we saw the normalized Scope 2 emissions increase. Even though many of our products became more complex, requiring additional manufacturing steps and hence more electricity to manufacture and test, our total Scope 2 emissions still decreased. These graphs are based on data that is calculated by the IEA conversion factors.
Renewable energy consumption from the energy grid mix, found in our energy chapter, reduces our Scope 2 emissions by 17% in 2019. However, the 17% renewable energy emissions reduction is not accounted for in the Normalized or Total Scope 2 emission graphs presented above. Therefore, our Scope 2 emissions are an overstatement. Corrections to 2019 and historical data for Scope 2 emissions will be made during 2020 to account for renewable energy consumption.
NXP’s Scope 3 emissions are reported for product transportation and business travel. From 2010 to 2019, the absolute Scope 3 emissions decreased by 46%.
In 2019, our CO2 emissions from transporting semi-finished products between factories, and from transporting fully finished products to warehouses and customers, was estimated at 16,332 tons CO2e (based on kilograms per km).
From 2010 to 2019 our product transportation emissions decreased by 31%. We are consolidating our central distribution centers and optimizing our shipping routes in which we contribute to the reduction of product transportation emissions. The standard value of reference for calculating airfreight CO2 is 0.567 kg per km. This is a value set by the Intergovernmental Panel on Climate Change (IPCC).
Business travel makes up a very small part of our CO2 emissions. Medium-and long-haul flights emit less CO2 per passenger km than short-haul flights, and rail travel is approximately 50% less CO2-intensive per passenger mile than air travel. Emissions from flights are calculated by using flight-distance categories (short, medium or long haul), along with the distance and average flight emission factors provided by the UK Department of Environment, Food and Rural Affairs (DEFRA) as of 2013.
Total CO2 emissions from business travel in 2019 was 11,492 tons of CO2e compared to the 2010 baseline of 23,732 tons of CO2e resulting in a 28% decrease.
For more information, please contact Corporate Environment Health & Safety.