Author

NXP
At NXP, innovation is always now, but our focus is always the future. Our dedicated team of experts is united by a passion to make everyday life more remarkable through technologies that continually redefine life as we know it.
Announced in March this year, the BBC’s micro:bit has been unveiled today. All the people excited by this fantastic initiative can now discover the final device and this extensive set of features on the BBC Make it Digital website. The micro:bit is a pocket-sized computer measuring 4cm by 5cm, and designed to be fun and easy to use. You can code, customize and control to bring your digital ideas, games and apps to life. It allows children and young people to develop an intuitive understanding of programming concepts and controlling hardware in technology and computing.
The micro:bit is one of the most ambitious STEM programs in recent years. It will be given freely to every child in year 7 or equivalent across the UK. The scale and scope of this unique initiative has only been made possible by an unprecedented collaboration between 28 international organizations, pioneering start-ups and transformative education organizations. The micro:bit’s products partners, amongst which Freescale, ARM, Microsoft, Samsung, Farnell have led on the software, hardware, design, manufacture and distribution of the device.
Specifically, Freescale has provided a Kinetis MCU and 2 motion sensors – a 3-axis accelerometer, and a 3-axis magnetometer. They allow the micro:bit to perform the following tasks:
These leading edge products embarked in the micro:bit are used in some of the most advanced devices available today on the market. They ensure the boards, while developed for children, are absolutely state of the art and will provide the perfect foundation on which future innovators can start building their skills.
—————————————–
Detailed specifications of the products Freescale donated for the micro:bit:
Kinetis KL26Z – 48 MHz, USB, Connectivity, Ultra-Low-Power MCU
The Kinetis KL26 MCU is part of the ultra-low-power Kinetis KL2x MCU family
based on the ARM® Cortex-M0+ core that includes a full-speed USB 2.0
On-the-Go (OTG) controller.
Target Applications
Features:
More information here.
MMA8653FC: ±2g/±4g/±8g, Low g, 10-Bit Digital
Accelerometer
The Freescale MMA8653FC 10-bit accelerometer has high performance
in a small DFN package. Packed with embedded functions that include:
Features
Target Applications
More information here.
MAG3110: Freescale High Accuracy, 3-Axis Magnetometer
The Freescale MAG3110 is a small, low-power digital 3-axis magnetic sensor
with a wide dynamic range to allow operation in PCBs with high extraneous
magnetic fields. The MAG3110:
Target Applications
More information here.
Tags: Connectivity, Technologies
At NXP, innovation is always now, but our focus is always the future. Our dedicated team of experts is united by a passion to make everyday life more remarkable through technologies that continually redefine life as we know it.
February 19, 2020
by NXP
March 23, 2020
June 3, 2020
by Lars Reger