Embedded Component specific for NXP® HC08 family LD64 and BD48 derivatives
This special Embedded Component implements a pulse-width modulation (PWM) generator with binary rate multiplier (BRM). Combining the 5-bit PWM together with the 3-bit BRM, the average duty cycle at the output will be (M+N/8)/32, where M is the content of the 5-bit PWM portion, and the N is the content of the 3-bit BRM portion.
Embedded Component specific for NXP HC08 family SR12 derivative
This special Embedded Component implements a pulse-width modulation (PWM) generator with three 8-bit channels. The automatic phase control feature allows phase delays between the channels. When automatic phase control is enabled, the PWM channel 2 will start immediately, but the channel 1 and channel 0 will be held in zero. After the counter of channel 2 reaches the phase value, the counter of channel 1 is released and starts counting. Finally, when the counter of channel 1 reaches the phase value, channel 0 is released and starts counting. It is possible to change the phase value for the channel 0 when the channel 1 has started its operation, before start of the channel 0 (use method SetPhaseReg).
Select a section:
This Embedded Component can be purchased for $125 and added to the Special and Standard Editions of CodeWarrior. Please note, this Embedded Component is included in the CodeWarrior Development Suite - Professional Edition.