Specialized Peripherals and Accelerators for NXP Microcontrollers

Overview

Features

PLU

PLU

SC Timer configuration

SC Timer configuration

Libraries and examples provided through MCUXpresso SDK

  • NXP has comprehensive enablement for the specialized interfaces and accelerators that differentiate its Arm Cortex-M-based microcontrollers. Each hardware feature is complemented with MCUXpresso SDK drivers and/or MCUXpresso configuration tool support, to help you complete an in-depth evaluation and get started with your design.

Programmable Logic

  • Available on LPC804 and select LPC5500 series MCUs
  • Design flows with Verilog, schematic capture or direct methods
  • Integration with MCUXpresso configuration tools

Coprocessors

  • PowerQuad DSP coprocessor for MCUs based on Cortex-M33 cores
  • CASPER security coprocessor for MCUs based on Cortex-M33 cores

Specialized Interfaces

  • Complex timing waveform generation
  • Intelligent peripherals
  • Highly efficient, low core overhead

Programmable Logic

The LPC804 MCU and several devices in the LPC5500 series incorporate a Programmable Logic unit (PLU) that can be used to implement a variety of interfaces and/or glue logic functions, reducing system component count and often greatly reducing processing load on the MCU itself. Logic designs for the PLU can be created using the complimentary PLU tool from NXP, which outputs register settings to be included in your application. Using the MCUXpresso configuration tools, you can configure and error check the connections from the PLU block to the device pins and check for connection errors, and simply drop your register settings into your application.

Devices with the PLU feature are shown below. Note that the SDK support for these boards can also be downloaded from within MCUXpresso IDE.

Device Family Core Programmable
Logic Unit
Recommended Evaluation Boards
LPC804 Cortex-M0+ LPCXpresso804
LPC55S6x Dual Cortex-M33 LPCXpresso55S69
LPC552x/S2x Cortex-M33 LPCXpresso55S28
LPC551x/S1x Cortex-M33 LPCXpresso55S16

Coprocessors

Arm Cortex-M33 Coprocessor

The Armv8-M architecture includes support for coprocessor extensions, and NXP has used this capability to develop highly efficient extensions for DSP and security-related processing.

PowerQuad Coprocessor

PowerQuad is a coprocessor designed by NXP to improve energy efficiency and performance when implementing DSP algorithms using its MCUs based on Cortex-M33 core. PowerQuad can be programmed directly or via an API that is compatible with Arm’s CMSIS-DSP library. MCUXpresso SDK includes API header files to support CMSIS-DSP, plus several examples showing their use.

Supported CMSIS-DSP API calls include:

  • Matrix functions
    • arm_mat_add_q15, arm_mat_add_q31, arm_mat_add_f32
    • arm_mat_sub_q15, arm_mat_sub_q31, arm_mat_sub_f32
    • arm_mat_mult_q15, arm_mat_mult_q31, arm_mat_mult_f32
    • arm_mat_inverse_f32
    • arm_mat_trans_q15, arm_mat_trans_q31, arm_mat_trans_f32
    • arm_mat_scale_q15, arm_mat_scale_q31, arm_mat_scale_f32
  • Math functions
    • arm_sqrt_q15, arm_sqrt_q31
    • arm_sin_q15, arm_sin_q31, arm_sin_f32
    • arm_cos_q15, arm_cos_q31, arm_cos_f32
  • Filter functions
    • arm_fir_q15, arm_fir_q31, arm_fir_f32
    • arm_conv_q15, arm_conv_q31, arm_conv_f32
    • arm_correlate_q15, arm_correlate_q31, arm_correlate_f32
  • Transform functions
    • arm_rfft_q15, arm_rfft_q31
    • arm_cfft_q15, arm_cfft_q31
    • arm_ifft_q15, arm_ifft_q31
    • arm_dct4_q15, arm_dct4_q31

PowerQuad has other hardware capabilities, such as transcendental functions, and examples of using these are also provided in the SDK.

Devices with PowerQuad are shown below. Note that the SDK support for these boards can also be downloaded from within MCUXpresso IDE.

Device Family Cores Recommended Evaluation Boards
LPC55S6x Dual Cortex-M33 LPCXpresso55S69
i.MX RT685 Cortex-M33 and Cadence® Tensilica® HiFi 4 DSP MIMXRT685-EVK

CASPER

To address the challenges of asymmetric cryptography, NXP has developed CASPER, a Cryptographic Accelerator and Signaling Processing Engine with RAM-sharing. It is a hardware accelerator engine for certain asymmetric cryptographic algorithms, such as Elliptic Curve Cryptography (ECC). CASPER sits on the Cortex-M33 coprocessor buses. CASPER is utilized by NXP’s implementation of MbedTLS in MCUXpresso SDK, so you can take advantage of the speed and energy-saving benefits with no additional effort compared to a software-only approach.

Devices with CASPER are shown below. Note that the SDK support for these boards can also be downloaded from within MCUXpresso IDE.

Device Family Cores Recommended Evaluation Boards
LPC55S6x Dual Cortex-M33 LPCXpresso55S69
i.MX RT685 Cortex-M33 and Cadence Tensilica HiFi 4 DSP MIMXRT685-EVK

Specialized Interfaces

NXP microcontrollers include powerful, innovative interface peripherals to reduce system cost, improve energy consumption and leave more processor cycles for your application.

Interface Block

LPC5500 series MCUs incorporate a specialized, programmable peripheral block that can be used to implement a variety of interfaces with little or zero overhead for the Arm cores they contain, enabling you to implement lower system cost implementations, save energy and leave more processing cycles for your applications. NXP provides drivers and examples for some specialized peripherals (upon request) that can be used with MCUXpresso SDK projects.

Devices with this specialized peripheral block feature are shown below.

Device Family Cores Keyboard
Scanner
Rotary
Encoder
Recommended Evaluation Boards
LPC55S6x Dual Cortex-M33 LPCXpresso55S69
LPC552x/S2x Cortex-M33 LPCXpresso55S28
LPC551x/S1x Cortex-M33 LPCXpresso55S16

State-controlled Timers

Several MCUs in NXP’s portfolio include powerful peripherals that can solve many logic and timing challenges.

The State Configurable Timer (SCT) is available on most LPC and i.MX RT600 microcontrollers. At its core, the SCT is a up/down counter that can be sequenced with up to 16 events on LPC5500 series devices (the number of events supported varies with the device family). The events can be triggered by IO or by one of 16 possible counter matches. An event can then update a state variable, generate IO activity (set, clear, toggle) or start/stop/reverse the counter. In some cases, the SCT can be used to build a semiautonomous subsystem, with very low MCU overhead to manage it. Using these capabilities, a broad range of sophisticated system designs can be implemented, often achieving system cost savings by reducing the need for external FPGAs or other components. MCUXpresso SDK includes examples of PWM timer implementations using the SCT, and the MCUXpresso Peripheral Configuration Tool enables design of state machine-controlled timers on-the-fly.

FlexIO Module

The FlexIO module is available in several members of the K32, Kinetis, i.MX RT MCU families. The FlexIO module is very flexible, allowing you to configure it according to your communication needs; it is capable of emulating various serial communication protocols such as UART, SPI and I2C. The main components of the FlexIO module are the shifters, timers and pins; data is loaded onto a shifter and a timer is assigned to generate the shifter clock and use a pin to input/output the data to/from the shifter. Shifters have a timer assigned to them to generate the shift clock and it can be configured to shift data in or out. Beyond serial interfaces, FlexIO can also emulate parallel interfaces, such as LCD display drivers, with very low MCU overheard. Examples using FlexIO to emulate I2C, I2S, UART, SPI and displays that match the 8080 and 6800 bus protocols are included in MCUXpresso SDK and Peripheral configuration tools, along with PWM driver examples. Examples for camera interfaces and IrDA camera interfaces are available in application notes from the NXP website by searching for “FlexIO application note”.

The table below shows which devices include the SCT and/or FlexIO special peripherals.

Device Family Cores FlexIO SCT
K8x, K27/28 Cortex-M4 -
KE1xx Cortex-M4/M0+ / Cortex-M0+ -
KL (excl. KL0x) Cortex-M0+ -
K32 L Cortex-M4/M0+ / Cortex-M0+ -
i.MX RT1010 Cortex-M7 -
i.MX RT1020 Cortex-M7 -
i.MX RT1050 Cortex-M7 -
i.MX RT1060 Cortex-M7 -
i.MX RT1160 Cortex-M7 / Cortex-M4 -
i.MX RT1170 Cortex-M7 / Cortex-M4 -
LPC81x/82x/83/x84x Cortex-M0 / M0+ -
LPC51U68 Cortex-M0+ -
LPC54000 Cortex-M4 -
LPC5500 Cortex-M33 / Dual Cortex-M33 -
i.MX RT500 Cortex-M33 / Cadence Tensilica Fusion F1 DSP
i.MX RT600 Cortex-M33 / Cadence Tensilica HiFi 4 DSP -