PTP Daemon Version 2 Build and Installation Instructions

05 January 2012

George V. Neville-Neil

The PTP Daemon is known to work on FreeBSD, NetBSD, Mac OS X and Linux systems.

*) Building 

1) cd into the src/ directory
3) Run "make"
4) Read the manual page.
5) Test it in place: ./ptpd2 -your -arguments -here
6) Run "make install"

The daemon may work on other Posix based systems but this is not
guaranteed.  Patches and fixes are welcome on the source forge page

http://ptpd.sf.net

or via mail to gnn@freebsd.org