Overview
========
The Hello World demo application provides a sanity check for the new SDK build environments and board bring up. The Hello
World demo prints the "Hello World" string to the terminal using the SDK UART drivers. The purpose of this demo is to
show how to use the UART, and to provide a simple project for debugging and further development.

Toolchain supported
===================
- IAR embedded Workbench  8.40.2
- Keil MDK  5.27
- GCC ARM Embedded  8.2.1
- MCUXpresso  11.0.1

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55s69 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
Note: MCUXpresso IDE project default debug console is semihost
1.  Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
2.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the hello world demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
hello world.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Customization options
=====================