Overview
========
The Hello World demo application provides a sanity check for the new SDK build environments and board bring up. The Hello
World demo prints the "Hello World" string to the terminal using the SDK UART drivers. The purpose of this demo is to
show how to use the UART, and to provide a simple project for debugging and further development.

Toolchain supported
===================
- IAR embedded Workbench  8.32.3
- Keil MDK  5.27
- GCC ARM Embedded  8.2.1
- MCUXpresso  11.0.0

Hardware requirements
=====================
- Mini/micro USB cable
- EVK-MIMXRT1060 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a USB cable between the host PC and the OpenSDA USB port on the target board. 
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows the output of the hello world demo in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
hello world.
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

Note:
To download binary into qspiflash and boot from qspiflash directly, following steps are needed:
1. Compile flash target of the project, and get the binaray file "hello_world.bin".
3. Set the SW7: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
4. Drop the binaray into disk "RT1060-EVK" on PC.
5. Wait for the disk disappear and appear again which will take couple of seconds.
7. Reset the board by pressing SW3 or power off and on the board. 
Customization options
=====================