Overview
========
The lpuart_edma Example project is to demonstrate usage of the KSDK lpuart driver.
In the example, you can send characters to the console back and they will be printed out onto console
 in a group of 8 characters.

Toolchain supported
===================
- IAR embedded Workbench  8.32.3
- Keil MDK  5.27
- GCC ARM Embedded  8.2.1
- MCUXpresso  11.0.0

Hardware requirements
=====================
- Mini/micro USB cable
- EVK-MIMXRT1060 board
- Personal Computer

Board settings
==============
No special settings are required.

Prepare the Demo
================
1.  Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

~~~~~~~~~~~~~~~~~~~~~~~~~~~
LPUART EDMA example
Send back received data
Echo every 8 characters
~~~~~~~~~~~~~~~~~~~~~~~~~~~
Customization options
=====================