Release Name: frdmkw36_TempCollOtap_wireless_example
Release Version: 1.0.0
Package License: LA_OPT_NXP_Software_License.htm - Production Use, Section 2.3 applies

CMSIS Core header files    Author: ARM                                       
                           parentversion: 4.5                                
                           URL: http://silver.arm.com                        
                           name: CMSIS Core header files                     
                           Format: source code                               
                           License: Open Source - BSD-3-Clause               
                           Location: <rootfolder>/CMSIS                           
                           version: 4.3 (CMSIS Download 4.5)                 
                           Description: Industry-standard header files       
                              distributed by ARM for cortex-M cores                                                                                                      

FreeRTOS(tm)               Author: Real Time Engineers, Ltd.                 
                           URL: http://www.freertos.org                      
                           name: FreeRTOS(tm)                                
                           Format: source code                               
                           License: Modified GPLv2. See                      
                              ,<rootfolder>/freertos/license.txt.  
                           Location: rtos/freertos_9.0.0                     
                           version: 9.0.0                                         
                           Description: A real-time operating system(RTOS)   
                              from Real Time Engineers, Ltd.                    

KSDK Peripheral Driver     Author: Freescale Semiconductors, Inc.
                           Format: source code                               
                           License: Open Source - BSD-3-Clause               
                           Location: <rootfolder>/drivers
                           Version: 2.x.x                                    
                           Description: Peripheral drivers are designed for  
                              the most common use cases indentified for         
                              the underlying hardware block.                    
                                       

Kinetis_BLE                Author: NXP
                           name: Bluetooth Low Energy Application Source     
                           Format: Source code and header Files              
                           License: Open Source - BSD-3-Clause               
                           Location: <rootfolder>/bluetooth     
                           version: 1.3.6                                    
                           Description: Bluetooth Low Energy Software        
                           Origin: NXP                                       

Kinetis_BLE_ControllerLib  Author: Mindtree
                           name: Bluetooth Low Energy Controller Firmware    
                           Format: Binary libraries                          
                           License: Proprietary, LA_OPT_NXP_Software_License 
                              - Production Use, Section 2.3 applies             
                           Location: <rootfolder>/libs
                           version: 4.2.6                                    
                           Description: Bluetooth Low Energy Controller      
                           Firmware. Host Command Interface (HCI).           
                           Origin: Mindtree                                  

Kinetis_BLE_HostLib        Author: NXP
                           name: Bluetooth Low Energy Host Firmware          
                           Format: Binary libraries                                                           
                           License: Proprietary, LA_OPT_NXP_Software_License 
                              - Production Use, Section 2.3 applies             
                           Location: <rootfolder>/libs      
                           version: 1.3.6                                    
                           Description: Bluetooth Low Energy Stack (HCI,     
                              L2CAP, ATT, GATT, GAP and SM)                     
                           Origin: NXP                                       

Kinetis_FWK                Author: NXP
                           name: Kinetis Connectivity Framework              
                           Format: Source code                                                                    
                           License: Open Source - BSD-3-Clause               
                           Location: <rootfolder>/framework    
                           version: 5.4.6                                    
                           Description: Kinetis Connectivity Framework       
                              middleware for Connectivity stacks                
                           Origin: NXP                                       

Kinetis_SecLib             Author: NXP
                           name: Kinetis Connectivity SecLib                 
                           Format: Binary libraries                                                        
                           License: Proprietary, LA_OPT_NXP_Software_License 
                              - Production Use, Section 2.3 applies             
                           Location: <rootfolder>/libs/lib_crypto_*.a                                 
                           version: 5.4.6                                    
                           Description: Connectivity Security Library for    
                              Kinetis                                           
                           Origin: NXP