NXP FreeMASTER Communication Driver
================================================================================

FreeMASTER is a PC-based application serving as a real-time monitor, visualization 
tool, and a graphical control panel of embedded applications based on NXP 
microcontroller and microprocessor units. The FreeMASTER Serial Communication 
Driver implements the serial interface between the target application and the host PC. 
The driver targets Serial and CAN communication of the supported devices.

This is version 3.1 of the serial driver which implements a new version (v4) of
FreeMASTER protocol and is compatible with NXP MCUXpresso SDK suite. The driver 
may be obtained as an MCUXpresso SDK middleware component at 
https://mcuxpresso.nxp.com/en/welcome.

Older implementations of FreeMASTER serial driver for platforms that are not 
supported by MCUXpresso SDK (e.g. HCS08, HCS12, S12Z, ColdFire, 56F8xxx) can 
be downloaded from FreeMASTER home at https://www.nxp.com/freemaster.

Visit community support forum at: https://community.nxp.com/community/freemaster  


CHANGELOG version 3.x versions
==============================

Version 3.1 (April 4th 2020)
----------------------------
- Use with FreeMASTER 2.5 and FreeMASTER 3.0 PC host tool or with FreeMASTER Lite
- Support for non-C99 compilers added
- Memory copy routines optimized for both little and big endian systems.
- New Kinetis, LPC and i.MX-RT devices directly supported in MCUXpresso SDK.
  Majority of MCUXpresso SDK boards now supported.
- The driver primarily supports CortexM platform, this version also adds support of 
  Power Architecture, S32, S12Z and DSC56F800EX platforms. Example applications 
  are available separately.  


Version 3.0 (April 29th 2019)
----------------------------
- The first release as MCUXpresso SDK middleware component
- Communication protocol completely redesigned (protocol version 4)
- Use FreeMASTER 2.5 or later to connect to microcontroller
- Example applications available for representative members of 
  Kinetis, LPC and i.MX-RT families of NXP microcontrollers:
      - FRDM-K64F
      - TWR-K64F
      - FRDM-KL28Z
      - FRDM-KE15Z
      - EVK-MIMXRT1060
      - LPCXPRESSO54628
      - LPCXPRESSO55S69
      - LPC845max



--------------------------------------------------------------------------------
Copyright 2019-2020 NXP
ALL RIGHTS RESERVED
www.nxp.com/freemaster