# SDK version.
PROJECT_NUMBER = "4.0.0b1"

# Doxygen layout file for libraries.
LAYOUT_FILE = doc/config/layout_library.xml

# Documentation output directory.
OUTPUT_DIRECTORY = doc/output/

# Don't generate LaTeX documentation
GENERATE_LATEX = NO

# Directories containing images.
IMAGE_PATH = doc/plantuml/images

# Don't rearrange members in the input files.
SORT_MEMBER_DOCS = NO

# Silence output (warnings only).
QUIET = YES

# Define the following preprocessor constants when generating documentation.
PREDEFINED = "DOXYGEN=1" \
             "IOT_STATIC_MEMORY_ONLY=1" \
             "LIBRARY_LOG_LEVEL=IOT_LOG_DEBUG" \
             "LIBRARY_LOG_NAME=\"DOXYGEN\""

# Ignore the constants used for setting log levels and names.
EXCLUDE_SYMBOLS = "LIBRARY_LOG_*"

# Configure Doxygen for C.
OPTIMIZE_OUTPUT_FOR_C = YES
TYPEDEF_HIDES_STRUCT = YES
EXTRACT_STATIC = YES

# Disable the tab bar and use treeview instead.
DISABLE_INDEX = YES
GENERATE_TREEVIEW = YES

# All files should have unique names, so showing the full path is unnecessary.
FULL_PATH_NAMES = NO

# Disable the default Doxygen diagrams.
HAVE_DOT = NO

# Disable the default Doxygen search engine (for now).
SEARCHENGINE = NO

# Use custom header file, footer file, and stylesheet.
HTML_HEADER = doc/config/html/header.html
HTML_FOOTER = doc/config/html/footer.html
HTML_EXTRA_STYLESHEET = doc/config/html/style.css

# Don't show external pages or groups.
EXTERNAL_GROUPS = NO
EXTERNAL_PAGES = NO

# Enable expansion of Unity test macros.
ENABLE_PREPROCESSING = YES
MACRO_EXPANSION = YES
EXPAND_ONLY_PREDEF = YES

# Expand the TEST macro, but ignore the _run functions generated from macro expansion.
EXPAND_AS_DEFINED = TEST
EXCLUDE_SYMBOLS += "TEST_*_run"

#Custom command
ALIASES += sideeffect="\par Side Effects"

# Alias for starting a dependencies section.
ALIASES += dependencies_section{1}="@section \1_dependencies Dependencies"
ALIASES += dependencies_brief{1}="@brief Dependencies of the \1."

# Alias for starting a configuration settings page.
ALIASES += describeconfig="Configuration settings are C pre-processor constants. They can be set with a @c #`define` in the iot_config.h or by using a compiler option such as `-D` in gcc. If a configuration setting is not defined, the library will use a \"sensible\" default value (unless otherwise noted). Because they are compile-time constants, a library must be rebuilt if a configuration setting is changed."

ALIASES += config_page{1}="@page \1_config Configuration"
ALIASES += config_page{2}="@page \1_config \2 Configuration"

ALIASES += config_brief{1}="@brief Configuration settings of the \1.<br>@describeconfig @par configpagemarker"
ALIASES += config_brief{3}="@brief Configuration settings of the \2.<br>@describeconfig<br><br>The settings on this page only affect the [\2](@ref \1). In addition to the settings on this page, the \2 will also be affected by [settings that affect all \3](@ref global_\3_config).@par configpagemarker"

# Aliases for "Possible values", "Recommended values", and "Default values"
# used in configuration setting pages.
ALIASES += configpossible="<b>Possible values:</b> "
ALIASES += configrecommended="<b>Recommended values:</b> "
ALIASES += configdefault="<b>Default value (if undefined):</b> "

# Alias for starting a constants page.
ALIASES += constants_page{1}="@page \1_constants Constants"
ALIASES += constants_brief{1}="@brief Defined constants of the \1.<br><br>Libraries may @c #`define` constants in their headers with special meanings. This page describes the meanings and uses of any constants defined by the \1. Related constants are shown in a single section on this page.<br>"

# Alias for starting a functions page.
ALIASES += functions_page{2}="@page \1_functions Functions"
ALIASES += functions_brief{1}="@brief Functions of the \1 library.<br><br>The \1 library consists of the following functions."
ALIASES += functions_page{3}="@page \1_functions \3"

# Alias for listing a single function on a functions page.
ALIASES += function_name{1}="@subpage \1"
ALIASES += function_brief{1}="<br>@copybrief \1"

# Alias for creating a page for a single function.
ALIASES += function_page{3}="@page \2_function_\3 \1"
ALIASES += function_snippet{3}="@snippet \3 declare_\1_\2"

# Alias for starting a handles group.
ALIASES += handles_group{1}="@defgroup \1_datatypes_handles Handles"
ALIASES += handles_brief{1}="@brief Opaque handles of the \1."

# Alias for starting an enum group.
ALIASES += enums_group{1}="@defgroup \1_datatypes_enums Enumerated types"
ALIASES += enums_brief{1}="@brief Enumerated types of the \1."

# Alias for starting a function pointers group.
ALIASES += functionpointers_group{1}="@defgroup \1_datatypes_functionpointers Function pointer types"
ALIASES += functionpointers_brief{1}="@brief Function pointer types of the \1."

# Alias for starting a structs group.
ALIASES += structs_group{1}="@defgroup \1_datatypes_structs Structured types"
ALIASES += structs_brief{1}="@brief Structured types of the \1."

# Alias for starting a parameter structures group.
ALIASES += paramstructs_group{1}="@defgroup \1_datatypes_paramstructs Parameter structures"
ALIASES += paramstructs_brief{2}="@brief Structures passed as parameters to [\2 functions](@ref \1_functions)<br>These structures are passed as parameters to library functions. Documentation for these structures will state the functions associated with each parameter structure and the purpose of each member."

# Alias for starting a return structures group.
ALIASES += returnstructs_group{1}="@defgroup \1_datatypes_returnstructs Return structures"
ALIASES += returnstructs_brief{1}="@brief Structures returned from [\1 functions](@ref \1_functions)<br>These structures are returned from library functions. Documentation for these structures will state the functions associated with each parameter structure and the purpose of each member."

# Alias for "Parameter for".
ALIASES += paramfor="<b>Parameter for:</b> "

# Alias for parameter structure initializers.
ALIASES += initializer{2}="All instances of #\1 should be initialized with #\2.<br>"