![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
This is the complete list of members for erpc::MessageBuffer, including all inherited members.
| copy(const MessageBuffer *other) | erpc::MessageBuffer | |
| get(void) | erpc::MessageBuffer | inline |
| get(void) const | erpc::MessageBuffer | inline |
| getFree(void) const | erpc::MessageBuffer | inline |
| getLength(void) const | erpc::MessageBuffer | inline |
| getUsed(void) const | erpc::MessageBuffer | inline |
| MessageBuffer(void) | erpc::MessageBuffer | inline |
| MessageBuffer(uint8_t *buffer, uint16_t length) | erpc::MessageBuffer | inline |
| operator const uint8_t *(void) const | erpc::MessageBuffer | inline |
| operator uint8_t *(void) | erpc::MessageBuffer | inline |
| operator[](int index) | erpc::MessageBuffer | inline |
| operator[](int index) const | erpc::MessageBuffer | inline |
| read(uint16_t offset, void *data, uint32_t length) | erpc::MessageBuffer | |
| set(uint8_t *buffer, uint16_t length) | erpc::MessageBuffer | inline |
| setUsed(uint16_t used) | erpc::MessageBuffer | inline |
| swap(MessageBuffer *other) | erpc::MessageBuffer | |
| write(uint16_t offset, const void *data, uint32_t length) | erpc::MessageBuffer |