![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
Logging messages functionality. More...
#include <erpc_message_loggers.h>
Collaboration diagram for erpc::MessageLoggers:Public Member Functions | |
| MessageLoggers (void) | |
| Constructor. | |
| virtual | ~MessageLoggers (void) |
| Transport destructor. | |
| bool | addMessageLogger (Transport *transport) |
| This function add given transport to newly created MessageLogger object. More... | |
Protected Member Functions | |
| erpc_status_t | logMessage (MessageBuffer *msg) |
| This function add given transport to newly created MessageLogger object. More... | |
Protected Attributes | |
| MessageLogger * | m_logger |
Logging messages functionality.
| bool MessageLoggers::addMessageLogger | ( | Transport * | transport | ) |
This function add given transport to newly created MessageLogger object.
| [in] | transport | Transport used for logging messages |
| True | When transport was successfully added. |
| False | When transport wasn't added. |
|
protected |
This function add given transport to newly created MessageLogger object.
| [in] | msg | Buffer which will be logged. |
|
protected |
Pointer to first logger.