![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
This is the complete list of members for erpc::RPMsgTransport, including all inherited members.
| get_rpmsg_lite_instance(void) | erpc::RPMsgBaseTransport | inline |
| hasMessage(void) | erpc::RPMsgTransport | inlinevirtual |
| init(uint32_t src_addr, uint32_t dst_addr, void *base_address, uint32_t length, uint32_t rpmsg_link_id) | erpc::RPMsgTransport | virtual |
| init(uint32_t src_addr, uint32_t dst_addr, void *base_address, uint32_t rpmsg_link_id, void(*ready_cb)(void), char *nameservice_name) | erpc::RPMsgTransport | virtual |
| m_dst_addr | erpc::RPMsgTransport | protected |
| m_messageQueue | erpc::RPMsgTransport | protected |
| m_rpmsg_ept | erpc::RPMsgTransport | protected |
| m_rpmsg_ept_context | erpc::RPMsgTransport | protected |
| receive(MessageBuffer *message) | erpc::RPMsgTransport | virtual |
| rpmsg_read_cb(void *payload, uint32_t payload_len, uint32_t src, void *priv) | erpc::RPMsgTransport | protectedstatic |
| RPMsgBaseTransport(void) (defined in erpc::RPMsgBaseTransport) | erpc::RPMsgBaseTransport | inline |
| RPMsgTransport(void) | erpc::RPMsgTransport | |
| s_initialized | erpc::RPMsgBaseTransport | protectedstatic |
| s_rpmsg | erpc::RPMsgBaseTransport | protectedstatic |
| s_rpmsg_ctxt | erpc::RPMsgTransport | protectedstatic |
| send(MessageBuffer *message) | erpc::RPMsgTransport | virtual |
| setCrc16(Crc16 *crcImpl) | erpc::Transport | inlinevirtual |
| Transport(void) | erpc::Transport | inline |
| ~RPMsgBaseTransport(void) (defined in erpc::RPMsgBaseTransport) | erpc::RPMsgBaseTransport | inlinevirtual |
| ~RPMsgTransport(void) | erpc::RPMsgTransport | virtual |
| ~Transport(void) | erpc::Transport | inlinevirtual |