![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
This is the complete list of members for erpc::SerialTransport, including all inherited members.
| FramedTransport(void) | erpc::FramedTransport | |
| hasMessage(void) | erpc::Transport | inlinevirtual |
| init(uint8_t vtime, uint8_t vmin) | erpc::SerialTransport | |
| m_crcImpl | erpc::FramedTransport | protected |
| m_receiveLock | erpc::FramedTransport | protected |
| m_sendLock | erpc::FramedTransport | protected |
| receive(MessageBuffer *message) | erpc::FramedTransport | virtual |
| send(MessageBuffer *message) | erpc::FramedTransport | virtual |
| SerialTransport(const char *portName, speed_t baudRate) | erpc::SerialTransport | |
| setCrc16(Crc16 *crcImpl) | erpc::FramedTransport | virtual |
| Transport(void) | erpc::Transport | inline |
| ~FramedTransport(void) | erpc::FramedTransport | virtual |
| ~SerialTransport(void) | erpc::SerialTransport | virtual |
| ~Transport(void) | erpc::Transport | inlinevirtual |