![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
Serial transport layer for host PC. More...
#include <erpc_serial_transport.h>
Inheritance diagram for erpc::SerialTransport:
Collaboration diagram for erpc::SerialTransport:Public Member Functions | |
| SerialTransport (const char *portName, speed_t baudRate) | |
| Constructor. More... | |
| virtual | ~SerialTransport (void) |
| Destructor. | |
| erpc_status_t | init (uint8_t vtime, uint8_t vmin) |
| Initialize Serial peripheral. More... | |
Public Member Functions inherited from erpc::FramedTransport | |
| FramedTransport (void) | |
| Constructor. | |
| virtual | ~FramedTransport (void) |
| Codec destructor. | |
| virtual erpc_status_t | receive (MessageBuffer *message) |
| Receives an entire message. More... | |
| virtual erpc_status_t | send (MessageBuffer *message) |
| Function to send prepared message. More... | |
| virtual void | setCrc16 (Crc16 *crcImpl) |
| This functions sets the CRC-16 implementation. More... | |
Public Member Functions inherited from erpc::Transport | |
| Transport (void) | |
| Constructor. | |
| virtual | ~Transport (void) |
| Transport destructor. | |
| virtual bool | hasMessage (void) |
| Poll for an incoming message. More... | |
Additional Inherited Members | |
Protected Attributes inherited from erpc::FramedTransport | |
| Crc16 * | m_crcImpl |
| Mutex | m_sendLock |
| Mutex protecting send. | |
| Mutex | m_receiveLock |
| Mutex protecting receive. | |
Serial transport layer for host PC.
| SerialTransport::SerialTransport | ( | const char * | portName, |
| speed_t | baudRate | ||
| ) |
Constructor.
| [in] | portName | Port name. |
| [in] | baudRate | Baudrate. |
| erpc_status_t SerialTransport::init | ( | uint8_t | vtime, |
| uint8_t | vmin | ||
| ) |
Initialize Serial peripheral.
| [in] | vtime | Read timeout. |
| [in] | vmin | Read timeout min. |