![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
Very basic transport to send/receive messages via UART. More...
#include <erpc_uart_cmsis_transport.h>
Inheritance diagram for erpc::UartTransport:
Collaboration diagram for erpc::UartTransport:Public Member Functions | |
| UartTransport (ARM_DRIVER_USART *uartDrv) | |
| Constructor. More... | |
| virtual | ~UartTransport (void) |
| Destructor. | |
| virtual erpc_status_t | init (void) |
| Initialize CMSIS UART peripheral configuration structure with values specified in UartTransport constructor. More... | |
Public Member Functions inherited from erpc::FramedTransport | |
| FramedTransport (void) | |
| Constructor. | |
| virtual | ~FramedTransport (void) |
| Codec destructor. | |
| virtual erpc_status_t | receive (MessageBuffer *message) |
| Receives an entire message. More... | |
| virtual erpc_status_t | send (MessageBuffer *message) |
| Function to send prepared message. More... | |
| virtual void | setCrc16 (Crc16 *crcImpl) |
| This functions sets the CRC-16 implementation. More... | |
Public Member Functions inherited from erpc::Transport | |
| Transport (void) | |
| Constructor. | |
| virtual | ~Transport (void) |
| Transport destructor. | |
| virtual bool | hasMessage (void) |
| Poll for an incoming message. More... | |
Protected Attributes | |
| ARM_DRIVER_USART * | m_uartDrv |
Protected Attributes inherited from erpc::FramedTransport | |
| Crc16 * | m_crcImpl |
| Mutex | m_sendLock |
| Mutex protecting send. | |
| Mutex | m_receiveLock |
| Mutex protecting receive. | |
Additional Inherited Members |
Very basic transport to send/receive messages via UART.
| UartTransport::UartTransport | ( | ARM_DRIVER_USART * | uartDrv | ) |
Constructor.
| [in] | uartDrv | Cmsis uart. |
|
virtual |
Initialize CMSIS UART peripheral configuration structure with values specified in UartTransport constructor.
| kErpcStatus_InitFailed | When UART init function failed. |
| kErpcStatus_Success | When UART init function was executed successfully. |
|
protected |
Access structure of the USART Driver