![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
#include "erpc_common.h"#include "erpc_message_buffer.h"#include "erpc_transport.h"#include <cstring>#include <stdint.h>
Include dependency graph for erpc_codec.h:
This graph shows which files directly or indirectly include this file:Go to the source code of this file.
Classes | |
| class | erpc::Codec |
| Abstract serialization encoder/decoder interface. More... | |
| class | erpc::CodecFactory |
| Abstract interface for codec factory. More... | |
Typedefs | |
| typedef void * | erpc::funPtr |
| typedef funPtr * | erpc::arrayOfFunPtr |
Enumerations | |
| enum | erpc::message_type_t { kInvocationMessage, kOnewayMessage, kReplyMessage, kNotificationMessage } |
| Types of messages that can be encoded. | |