![]() |
eRPC API Reference
Rev. 1.7.4
NXP Semiconductors
|
#include "erpc_transport_setup.h"
Include dependency graph for erpc_mbf_setup.h:
This graph shows which files directly or indirectly include this file:Go to the source code of this file.
Typedefs | |
| typedef struct ErpcMessageBufferFactory * | erpc_mbf_t |
| Opaque MessageBufferFactory object type. | |
Functions | |
MessageBufferFactory setup | |
| erpc_mbf_t | erpc_mbf_static_init (void) |
| Create MessageBuffer factory which is using static allocated buffers. | |
| erpc_mbf_t | erpc_mbf_dynamic_init (void) |
| Create MessageBuffer factory which is using dynamic allocated buffers. | |
| erpc_mbf_t | erpc_mbf_rpmsg_init (erpc_transport_t transport) |
| Create MessageBuffer factory which is using RPMSG LITE zero copy buffers. More... | |
| erpc_mbf_t | erpc_mbf_rpmsg_tty_init (erpc_transport_t transport) |
| Create MessageBuffer factory which is using RPMSG LITE TTY buffers. More... | |